cyw43438 firmware will crash,and wlan down, when work on AP mode

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

Platform: linux2.6.32+compat-wireless-3.5.4-1, cyw43438

wifi mode :AP mode

This bug is not occured every time,and the time is not fixed,maybe halfhour or several hours.

Here is the log,

BCM:<6>CFG80211-ERROR) wl_cfg80211_set_channel : BCM:netdev_ifidx(6), chan_type(0) target channel(2)

BCM:<6>CFG80211-ERROR) wl_cfg80211_parse_ies : BCM:No WPSIE in beacon

BCM:<6>CFG80211-ERROR) wl_cfg80211_parse_ies : BCM:No WPSIE in beacon

BCM:_dhd_wlfc_mac_entry_update():1636, entry(32)

BCM:<6>CFG80211-ERROR) wl_notify_connect_status_ap : BCM:event WLC_E_DEAUTH_IND(6) status 0 reason 3

BCM:<6>CFG80211-ERROR) wl_notify_connect_status_ap : BCM:event WLC_E_DISASSOC_IND(12) status 0 reason 8

BCM:<6>CFG80211-ERROR) wl_notify_connect_status_ap : BCM:event WLC_E_DEAUTH(5) status 0 reason 4

BCM:<6>CFG80211-ERROR) wl_notify_connect_status_ap : BCM:event WLC_E_DISASSOC_IND(12) status 0 reason 8

BCM:INTERNAL ERROR: FIRMWARE HALTED : set BUS DOWN

BCM:CONSOLE: at 0x00af m_cts_duration 0x0000 m_ucode_dbgst 0x0002

BCM:CONSOLE: 002008.407      wepctl 0x0350, pcmctl 0x0300, pcmstat 0x0000

BCM:CONSOLE: 002008.407 M_RXFRM_BLK scr(0:63) btc_params(0:63) PC AXI slave error; APB Bridge 0

BCM:CONSOLE: 002008.407          errlog: lo 0x180013fe, hi 0x00000000, id 0x00040004, flags 0x00000100, status 0x00000005

BCM:CONSOLE: 002008.407

BCM:CONSOLE: FWID 01-f52710fa

BCM:CONSOLE: flags 1

BCM:CONSOLE: 002008.407

BCM:CONSOLE: TRAP 3(6fe40): pc c4f6, lr c4b3, sp 6fe94, cpsr 60000003, spsr 61000010

BCM:CONSOLE: 002008.407   r0 3, r1 ec9224, r2 0, r3 1f0, r4 59974, r5 18001000, r6 6ad74

BCM:CONSOLE: 002008.407   r7 40, r8 599f4, r9 6ff40, r10 18004000, r11 18104000, r12 0

BCM:CONSOLE: 002008.407

BCM:CONSOLE:    sp+0 00000003 00ec9224 00000000 000001f0

BCM:CONSOLE: 002008.407   sp+10 00000000 0000c4b3 0000c4f6 61000010

BCM:CONSOLE:

BCM:CONSOLE: 002008.408 sp+14 0000c4b3

BCM:CONSOLE: 002008.408 sp+4c 0000c539

BCM:CONSOLE: 002008.408 sp+68 00000413

BCM:CONSOLE: 002008.408 sp+6c 0000c5b3

BCM:CONSOLE: 002008.408 sp+7c 00022183

BCM:CONSOLE: 002008.408 sp+a4 00008325

BCM:CONSOLE: 002008.408 sp+c4 00002729

BCM:CONSOLE: 002008.408 sp+d4 00002e55

BCM:CONSOLE: 002008.408 sp+dc 00002029

BCM:CONSOLE: 002008.408 sp+128 00002a0b

BCM:CONSOLE: 002008.408 sp+148 00002a0b

BCM:CONSOLE: 002008.408 sp+158 0000221b

BCM:dhdsdio_checkdied: msgtrace address : 0x00000000

console address  : 0x0006DEBC

Assrt not built in dongle

Dongle trap type 0x3 @ epc 0xc4f6, cpsr 0x60000003, spsr 0x61000010, sp 0x6fe94,lp 0xc4b3, rpc 0xc4f6 Trap offset 0x6fe40, r0 0x3, r1 0xec9224, r2 0x0, r3 0x1f0, r4 0x59974, r5 0x18001000, r6 0x6ad74, r7 0x40

BCM:dhdsdio_dpc: failed backplane access over SDIO, halting operation

BCM:dhd_prot_ioctl : bus is down. we have nothing to do

BCM:dhd_check_hang: Event HANG send up due to  re=0 te=0 e=-1 s=0

BCM:dhd_check_hang: Event HANG send up due to  re=0 te=0 e=-1 s=0

BCM:<6>CFG80211-ERROR) wl_cfg80211_get_station : BCM:GET STA INFO failed, -1

(2000-01-05 04:28:16.033874511 UTC),dhd_stop: current comm: events/0, pid:432

0 Likes
1 Solution
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hi :

     For Linux it is better you can get the help from our account support team, it may need to try different DHD version, FW version,  and communication interface tuning .

View solution in original post

0 Likes
1 Reply
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hi :

     For Linux it is better you can get the help from our account support team, it may need to try different DHD version, FW version,  and communication interface tuning .

0 Likes