Wi-Fi Bluetooth for Linux Forum Discussions
Package Version
ahd-2023_1221
Release Date
2023-12-21
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform and Hikey960 PCIE platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* 4373-Android13-SDIO
*43012-Android13-SDIO
*43022-Android13-SDIO
*54591-Android13-PCIE
*55572-Android13-SDIO
*AHDBinaries
*device
*firmware
*nvram
* Android13_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
* confs
* hostapd_supplicant_src
* Android13_PCIE_Bringup.pdf
* Android13_SDIO_Bringup.pdf
* Android13_Feature_Bringup.pdf
Test Environment:
* IMX8 SDIO setup
* Hikey960 PCIE setup
* 55572, 43012, 43022, 54591 and 4373 Sanity, 6G and 11ax features (55572), WOWL via OOB(55572)
and PNO scan offload(55572, 43022)
Show LessDescription
The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code examples of Bluetooth® profiles) to evaluate and test Bluetooth® Classic and Low Energy on AIROC™ combo chip (CYW4373, CYW43439, CYW55573/2/1).
What's new?
Package comes with codes examples to demonstrate Bluetooth LE Audio capability of CYW55573/2/1 in hosted mode. The code example demonstrates Bluetooth® LE Audio unicast and broadcast functionality.
Functions include:
- Broadcast audio stream scanning
- Receiving broadcast audio stream
- Unicast audio stream establishment
- Unicast audio stream release
- Unicast sink connect to source (1 CIG, 1 CIS)
Bluetooth® Linux Code Examples & Supported Chip
Code example |
Feature demonstration |
Supported chip |
LE Audio CIS Source |
Implements the Unicast Source application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio CIS Sink |
Implements the Unicast Sink application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Source |
Demonstrates the ability of LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Sink |
Demonstrates the ability to receive LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® Find me |
Demonstrates the Find Me profile which defines the behavior when a button is pressed on one device to cause an alerting signal on a peer device |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® hello sensor |
Demonstrates GATT database and device configuration initialization, sending data to the client and processing write requests from the client |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Wi-Fi onboarding |
Demonstrates the feature that enables devices to connect to a Wi-Fi access point without requiring a physical interface |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Headset |
Multiple profile code example that demonstrates the use cases and ability of audio-related functions such as A2DP, AVRCP CT, and HFP |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® SPP |
Demonstrates how two devices can establish a wireless communication link that emulates a traditional serial port connection |
CYW43439,CYW4373 |
Package GitHub link: https://github.com/Infineon/ifx-linux-bluetooth
Release notes
Please go through the attached released notes for more details on the package.
Show Lessv5.15.58-2024_0118
Release Date
2024-01-18
Github Link
V5.15.58 backport package: Link
V6.1.19 patch: link
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
Part 1: cypress-fmac-v5.15.58-2023_1128.zip
* Backports package (cypress-backports-v5.15.58-2023_1128-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_1128.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_1128.tar.gz)
* Device tree files (cypress-devicetree-2023-11-28.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_1128.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Part 2: cypress-patch-v6.1.19-2023_1128.zip
* Cypress fmac patch files for Vanilla v6.1.19(cypress-patch-v6.1.19-2023_1128.tar.gz)
* Infineon-Vanilla-Kernel-v6.1.19-Bring-up-Reference_20201221.pdf
Checksum
cypress-fmac-v5.15.58-2023_1128 sha256sum:
990b5f6beeb9530525f254977569fd25936e09f9ef1bf36ca52118e73dff3e68 cypress-backports-v5.15.58-2023_1128-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
0c8da2efe289115f2242aa3f69de5bc616cb893ecd411e11194c4c008418bb2e cypress-custom-patch-5.4.21.tar.gz
c38cca05bb05db6198af7809c7a2e519cb33a06b02ebd4d626588c9038f7259b cypress-devicetree-2023-11-28.tar.gz
92608ceb4509cc02730833ce2119662b3c116a3956ca303245e97378186dc2a3 cypress-firmware-v5.15.58-2023_1128.tar.gz
771099830bd106307e77ebdd4d27a3e18de27bb60889c4db4bca81f44ade495d cypress-hostap_2_10-2023_1128.tar.gz
8fe7d8b677032fb04374615aae27c5a3131499956dc22ddb420847a3876974c6 cypress-patch-v5.15.58-2023_1128.tar.gz
cypress-patch-v6.1.19-2023_1128 sha256sum:
933ac3a50f0146b4078beb5e398c75a93ab0a1979a93d120a1c0ba2a06ab0ff7 Infineon-Kernel-v6.1.19-Bring-up-Reference.pdf
ac23fabed00e5c5ab0c3720fa0eb6fa135a589e009714f783701fe557abe3fe7 v6.1.19-2023_1128.tar.gz
Part 3: cypress-fmac-v5.15.58-2024_0118.zip
8ccbebf31bf69c85dc7d05fb7e3597fa282c3ba5373d76b2a65364191abb14d0 cypress-backports-v5.15.58-2024_0118-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
92e7196a896fa65138c8297d4202a1811564605360f807faa2c8af310eddeb2e cypress-custom-patch-5.4.21.tar.gz
40dd314cee28149028a2d524ccd5d25f20336c7314e1e26654daecf4c9a796d2 cypress-devicetree-2024-01-18.tar.gz
739d1fae54d885e136847af2957821324c18c68622f204992e268b991172da53 cypress-firmware-2024_0118.tar.gz
2a411fb64818b054498645f64e3ef3b29e4db9a36b65987d9a3af76c2d60f765 cypress-hostap_2_10-2024_0118.tar.gz
8e43bc4487c5d4e77880e2fc9d3152a011063c5b0f3871e277561f0108a88304 cypress-patch-v5.15.58-2024_0118.tar.gz
[Change Log]
2023-12-18 Initial Post
2023-12-22 Add cypress-patch-v6.1.19 to support build brcmfmac on 6.1.19
2024-01-18 Fix for system crash post suspend and resume with CYW55572/55573 [PCIe]
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now.
Description:
AIROC Bluetooth Stack is Infineon's Bluetooth Host Protocol Stack implementation. The stack is optimized to work with Infineon Bluetooth controllers. The BTSTACK supports Bluetooth BR/EDR and BLE core protocols. This page provides the Github links to get started with application developments in Linux platform using AIROC Bluetooth Stack.
Please find the code examples :
Code Examples:
https://github.com/Infineon/linux-example-btstack-wifi-onboarding
https://github.com/Infineon/linux-example-btstack-wakeonle
https://github.com/Infineon/linux-example-btstack-bas
https://github.com/Infineon/linux-example-btstack-hello-sensor
https://github.com/Infineon/linux-example-btstack-alert-client
https://github.com/Infineon/linux-example-btstack-alert-server
https://github.com/Infineon/linux-example-btstack-headset
https://github.com/Infineon/linux-example-btstack-a2dp-source
https://github.com/Infineon/linux-example-btstack-a2dp-sink
https://github.com/Infineon/linux-example-btstack-spp
https://github.com/Infineon/linux-example-btstack-handsfree-unit
https://github.com/Infineon/linux-example-btstack-handsfree-ag
Show Less
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here:
Sr. No. | Driver release name | Release link |
1 | Backports v5.15.58-2023_1128 |
Public forum link: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238 |
2 | 6.1 Latest kernel for RPI : RPI-6.1.21 IFXFMAC |
Github: https://github.com/Infineon/rpi-linux-kernel/releases/tag/6.1.21-hedorah-IFXFMAC-20231128 |
3 | 6.1 Kernel on BRCMFMAC |
Github: https://github.com/Infineon/ifx-wireless-drivers/tree/RTM/v6.1.19-hedorah |
Documentation is available in docs folder of cypress-fmac-v5.15.58-2023_1128.zip available at this link https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238
The older/archived Wi-Fi driver releases can be accessed here:
Show Less
Package Version
ahd-2022_1223
Release Date
2023-01-03
Description
Cypress Android release for the broad market.
This release has been qualified on Hikey 960 platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* ahd
* device
*hikey960
* firmware
* nvram
* 55572_AndroidBringup.pdf
Test Environment:
* Hikey 960
* 55572 Sanity and VTS
Change Log
[2022-12-23]
* Initial post
Show LessHi there,
We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor.
We need help to compile the wl_tool so we can proceed with certification, but we need it to be cross compiled for our architecture (arm 32bit).
Can I ask a representative to help us to compile it with our custom toolchain?
CPU Info:
- armv7l
- little-endian
- hard-float ABI
- neon/vfpv4
Custom Toolchain Instructions:
- download toolchain
- extract toolchain:
tar jxf arm-co6-linux-uclibcgnueabihf_sdk-buildroot_2021.02.1.tar.xz - cd to arm-co6-linux-uclibcgnueabihf_sdk-buildroot
- ./relocate_sdk.sh
- add toolchain into path e.g.
export PATH="$PATH:$PWD/usr/bin" - Set cross compile variables:
export ARCH=arm
export CROSS_COMPILE=arm-co6-linux-uclibcgnueabihf-
Tagging @VinayakS_26 / @raks_99 / @DoubleLo as I found they have helped another customer to do this.
Show Less
Hi Sir,
I was testing wl cmd,there were some error,please help to check,my cmd as below:
wl mpc 0
wl up
wl band b
wl channel 1
wl curpower
Error: read ppr board limit failed
Chip number:cyw43438
OS: Android 7.1
CPU: Allwinner
The attached are Doc and my actually test .
Thanks,
Leo
Show LessHi
Normally, in Linux systems, country specific frequency-band and power settings are defined and handled via regdb.
The 89359 brakepad driver uses a CLM blob to define band and power settings.
How is the relation of CLM to regdb in this driver? Are regdb values used by the driver or can the settings only be done via CLM blob?
Kind regards
Stefan
Show LessI'm used i.MX6UltraLite EVK with Murata 1mw module
I need to enable interworking tag(107) in Access Point, I have setup a configuration for hostapd that provide it but it is does not show up when i am scanning the Access Point, only custom Vendor Id seems supported"""
Show Lesshello:
cyw43340 OTP document is as follows:
1.What are the meanings of pa0b0,pa0b1 and pa0b2 respectively, and what are the validity of their respective parameters ?
How should we adjust the parameters according to our actual circuit ?
2. Pa1lob0,pa1b0, and pahib0 correspond to 5 GHz low-band, 5 GHz mid-band, and 5 GHz hi-band, respectively !
What is the frequency range corresponding to 5 GHz low-band, 5 GHz mid-band and 5 GHz hi-band respectively ?
We are using 43340 for rf performance test and have encountered some problems, so we want to know how to adjust it. We hope to get a reply as soon as possible. Thank you !
hello:
I am testing the receiving sensitivity in non-signaling mode. How to calculate the bit error rate according to the returned information,as follow:
I think there is no problem with the test method I used. I just don't know how to convert it,thanks!
Show Lesshello
cyw43340 Tx power can be adjusted,I have the following questions:
Refer to otp document:
maxp2ga0=0x46,max output power is 17.5dbm,the nominal power is 17.5 – 1.0 = 16.5 dBm.
What is the actual power output if the following configuration is used:
maxp2ga0=0x46
ofdm2gpo=0x44444444(back-off power is 2dbm)
when rate is 6Mbps,The actual output power should choose which of the following?
1.max output power(17.5)-2dbm =15.5 dbm
2.the nominal power(16.5) - 2 dbm = 14.5 dbm
think you!
Show Lesshello:
In the following two paths for wiced 6.4:
paths 1:43xxx_wifi/platforms/BCM943340WCD1/wifi_nvram.h
paths 2:43xxx_wifi/platforms/BCM943362WCD4/wifi_nvram.h
The following two parameters are different:
"edonthd=-65" "\x00"
"edoffthd=-71" "\x00"
Path 1 doesn't exist. Path 2 does
I want to know the meaning of these two parameters and their impact on wifi usage,thinks!
Show LessI'm looking to FCC certify a Nvidia Jetson TX2 product which uses the BCM4354 module. It appears that in order to put the module into continuous transmission mode, I require the "wl" utility. Unfortunately, the SDK that Nvidia provides does not include this utility.
I've located these two other posts that seem relevant:
https://community.cypress.com/message/144616#144616
https://community.cypress.com/message/199171#199171
Based on these posts, I have a precompiled ARM version of wl that is executable on the TX2, but it's not able to actually execute any commands. This leads me to believe that in order for wl to work, I require the bcmfmac driver instead of the bcmdhd driver that's currently used, but I can't find any documentation that confirms this.
Any help in acquiring a working wl tool would be greatly appreciated. Do I need to get bcmfmac loaded in order to do this?
Thanks,
Show LessIt seems that the Hardware TSF implemented by WiFi controllers is a useful source of a synchronized time datum across the devices connected to a single WiFi network.
I see that this question hardware timestamping about accessing TSF in an earlier WiFi chip received the negative response "Synchronizing TSF with host MCU is not supported on Wiced."
I would like to know if - and how - the CYW43455 TSF can be accessed by host software or driver (typical host might be RPI3B).
Thanks!
Show Less