Wi-Fi Bluetooth for Linux Forum Discussions
Package Version
ahd-2023_1221
Release Date
2023-12-21
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform and Hikey960 PCIE platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* 4373-Android13-SDIO
*43012-Android13-SDIO
*43022-Android13-SDIO
*54591-Android13-PCIE
*55572-Android13-SDIO
*AHDBinaries
*device
*firmware
*nvram
* Android13_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
* confs
* hostapd_supplicant_src
* Android13_PCIE_Bringup.pdf
* Android13_SDIO_Bringup.pdf
* Android13_Feature_Bringup.pdf
Test Environment:
* IMX8 SDIO setup
* Hikey960 PCIE setup
* 55572, 43012, 43022, 54591 and 4373 Sanity, 6G and 11ax features (55572), WOWL via OOB(55572)
and PNO scan offload(55572, 43022)
Show LessDescription
The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code examples of Bluetooth® profiles) to evaluate and test Bluetooth® Classic and Low Energy on AIROC™ combo chip (CYW4373, CYW43439, CYW55573/2/1).
What's new?
Package comes with codes examples to demonstrate Bluetooth LE Audio capability of CYW55573/2/1 in hosted mode. The code example demonstrates Bluetooth® LE Audio unicast and broadcast functionality.
Functions include:
- Broadcast audio stream scanning
- Receiving broadcast audio stream
- Unicast audio stream establishment
- Unicast audio stream release
- Unicast sink connect to source (1 CIG, 1 CIS)
Bluetooth® Linux Code Examples & Supported Chip
Code example |
Feature demonstration |
Supported chip |
LE Audio CIS Source |
Implements the Unicast Source application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio CIS Sink |
Implements the Unicast Sink application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Source |
Demonstrates the ability of LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Sink |
Demonstrates the ability to receive LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® Find me |
Demonstrates the Find Me profile which defines the behavior when a button is pressed on one device to cause an alerting signal on a peer device |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® hello sensor |
Demonstrates GATT database and device configuration initialization, sending data to the client and processing write requests from the client |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Wi-Fi onboarding |
Demonstrates the feature that enables devices to connect to a Wi-Fi access point without requiring a physical interface |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Headset |
Multiple profile code example that demonstrates the use cases and ability of audio-related functions such as A2DP, AVRCP CT, and HFP |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® SPP |
Demonstrates how two devices can establish a wireless communication link that emulates a traditional serial port connection |
CYW43439,CYW4373 |
Package GitHub link: https://github.com/Infineon/ifx-linux-bluetooth
Release notes
Please go through the attached released notes for more details on the package.
Show Lessv5.15.58-2024_0118
Release Date
2024-01-18
Github Link
V5.15.58 backport package: Link
V6.1.19 patch: link
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
Part 1: cypress-fmac-v5.15.58-2023_1128.zip
* Backports package (cypress-backports-v5.15.58-2023_1128-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_1128.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_1128.tar.gz)
* Device tree files (cypress-devicetree-2023-11-28.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_1128.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Part 2: cypress-patch-v6.1.19-2023_1128.zip
* Cypress fmac patch files for Vanilla v6.1.19(cypress-patch-v6.1.19-2023_1128.tar.gz)
* Infineon-Vanilla-Kernel-v6.1.19-Bring-up-Reference_20201221.pdf
Checksum
cypress-fmac-v5.15.58-2023_1128 sha256sum:
990b5f6beeb9530525f254977569fd25936e09f9ef1bf36ca52118e73dff3e68 cypress-backports-v5.15.58-2023_1128-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
0c8da2efe289115f2242aa3f69de5bc616cb893ecd411e11194c4c008418bb2e cypress-custom-patch-5.4.21.tar.gz
c38cca05bb05db6198af7809c7a2e519cb33a06b02ebd4d626588c9038f7259b cypress-devicetree-2023-11-28.tar.gz
92608ceb4509cc02730833ce2119662b3c116a3956ca303245e97378186dc2a3 cypress-firmware-v5.15.58-2023_1128.tar.gz
771099830bd106307e77ebdd4d27a3e18de27bb60889c4db4bca81f44ade495d cypress-hostap_2_10-2023_1128.tar.gz
8fe7d8b677032fb04374615aae27c5a3131499956dc22ddb420847a3876974c6 cypress-patch-v5.15.58-2023_1128.tar.gz
cypress-patch-v6.1.19-2023_1128 sha256sum:
933ac3a50f0146b4078beb5e398c75a93ab0a1979a93d120a1c0ba2a06ab0ff7 Infineon-Kernel-v6.1.19-Bring-up-Reference.pdf
ac23fabed00e5c5ab0c3720fa0eb6fa135a589e009714f783701fe557abe3fe7 v6.1.19-2023_1128.tar.gz
Part 3: cypress-fmac-v5.15.58-2024_0118.zip
8ccbebf31bf69c85dc7d05fb7e3597fa282c3ba5373d76b2a65364191abb14d0 cypress-backports-v5.15.58-2024_0118-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
92e7196a896fa65138c8297d4202a1811564605360f807faa2c8af310eddeb2e cypress-custom-patch-5.4.21.tar.gz
40dd314cee28149028a2d524ccd5d25f20336c7314e1e26654daecf4c9a796d2 cypress-devicetree-2024-01-18.tar.gz
739d1fae54d885e136847af2957821324c18c68622f204992e268b991172da53 cypress-firmware-2024_0118.tar.gz
2a411fb64818b054498645f64e3ef3b29e4db9a36b65987d9a3af76c2d60f765 cypress-hostap_2_10-2024_0118.tar.gz
8e43bc4487c5d4e77880e2fc9d3152a011063c5b0f3871e277561f0108a88304 cypress-patch-v5.15.58-2024_0118.tar.gz
[Change Log]
2023-12-18 Initial Post
2023-12-22 Add cypress-patch-v6.1.19 to support build brcmfmac on 6.1.19
2024-01-18 Fix for system crash post suspend and resume with CYW55572/55573 [PCIe]
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now.
Description:
AIROC Bluetooth Stack is Infineon's Bluetooth Host Protocol Stack implementation. The stack is optimized to work with Infineon Bluetooth controllers. The BTSTACK supports Bluetooth BR/EDR and BLE core protocols. This page provides the Github links to get started with application developments in Linux platform using AIROC Bluetooth Stack.
Please find the code examples :
Code Examples:
https://github.com/Infineon/linux-example-btstack-wifi-onboarding
https://github.com/Infineon/linux-example-btstack-wakeonle
https://github.com/Infineon/linux-example-btstack-bas
https://github.com/Infineon/linux-example-btstack-hello-sensor
https://github.com/Infineon/linux-example-btstack-alert-client
https://github.com/Infineon/linux-example-btstack-alert-server
https://github.com/Infineon/linux-example-btstack-headset
https://github.com/Infineon/linux-example-btstack-a2dp-source
https://github.com/Infineon/linux-example-btstack-a2dp-sink
https://github.com/Infineon/linux-example-btstack-spp
https://github.com/Infineon/linux-example-btstack-handsfree-unit
https://github.com/Infineon/linux-example-btstack-handsfree-ag
Show Less
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here:
Sr. No. | Driver release name | Release link |
1 | Backports v5.15.58-2023_1128 |
Public forum link: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238 |
2 | 6.1 Latest kernel for RPI : RPI-6.1.21 IFXFMAC |
Github: https://github.com/Infineon/rpi-linux-kernel/releases/tag/6.1.21-hedorah-IFXFMAC-20231128 |
3 | 6.1 Kernel on BRCMFMAC |
Github: https://github.com/Infineon/ifx-wireless-drivers/tree/RTM/v6.1.19-hedorah |
Documentation is available in docs folder of cypress-fmac-v5.15.58-2023_1128.zip available at this link https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238
The older/archived Wi-Fi driver releases can be accessed here:
Show Less
Package Version
ahd-2022_1223
Release Date
2023-01-03
Description
Cypress Android release for the broad market.
This release has been qualified on Hikey 960 platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* ahd
* device
*hikey960
* firmware
* nvram
* 55572_AndroidBringup.pdf
Test Environment:
* Hikey 960
* 55572 Sanity and VTS
Change Log
[2022-12-23]
* Initial post
Show LessHi there,
We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor.
We need help to compile the wl_tool so we can proceed with certification, but we need it to be cross compiled for our architecture (arm 32bit).
Can I ask a representative to help us to compile it with our custom toolchain?
CPU Info:
- armv7l
- little-endian
- hard-float ABI
- neon/vfpv4
Custom Toolchain Instructions:
- download toolchain
- extract toolchain:
tar jxf arm-co6-linux-uclibcgnueabihf_sdk-buildroot_2021.02.1.tar.xz - cd to arm-co6-linux-uclibcgnueabihf_sdk-buildroot
- ./relocate_sdk.sh
- add toolchain into path e.g.
export PATH="$PATH:$PWD/usr/bin" - Set cross compile variables:
export ARCH=arm
export CROSS_COMPILE=arm-co6-linux-uclibcgnueabihf-
Tagging @VinayakS_26 / @raks_99 / @DoubleLo as I found they have helped another customer to do this.
Show Less
I have a client using the warp7 board with murata 1DX module with Cypress/CYW4343W.
https://www.element14.com/community/community/designcenter/single-board-computers/warp7
Is this supported with the latest FMAC driver? I built a kernel with the latest FMAC [2019-10-31] following the README for Linux Stable v4.14.77 but when I run it I get an error in the log that it failed to load the firmware .bin file and I don't see the wireless come up.
If I build with the freescale community bsp (Yocto thud) which supports the board (imx7s-warp), I get a linux 4.20.0-rc6 kernel with a brcmfmac driver, is that just an older FMAC driver?
This is similar to this discussion post by GrahamS_21 which is locked but was not answered publicly.
"I have a customer trying to use the iMX7s-warp board, which has a type-1dx module (CYW4343W)
Our latest FMAC driver and firmware supports kernel 4.1.15 which has no MACHINE imx7s-warp
They imported the Yocto meta-layer for the imx7s-warp from another BSP but this overrides the preferred kernel and pulls in 4.1.32 in which then it becomes a kernel source/header file headache for FMAC.
The current Yocto BSPs all support the imx7s-warp ( 4.1.32 up ) and have the bcmdhd and brcmfmac drivers within, the brcmfmac doesn't actually work but as it's close to FMAC as far as I know - it may be a good starting point for a possible port?
Can we provide some guidance on how to enable this feature? for reference this works ok on the iMX7d board, just not the WARP one."
We want to use the latest driver to help diagnose or prevent some connection issues that were observed with an older kernel and driver.
Regards,
Aaron
Show LessHello everyone, when I designed the board using the BCM43438, I started the WL_REG_ON this pin and thought that the chip should have worked properly and that the measurement of each voltage was correct. But when I measured the voltage at both ends of the crystal, I found that there was no voltage, what was the reason? I use what seems to be the official recommendation of 37.4MHz crystal and 12pF capacitor.
Show LessHi,
This question is related to the following discussion.
Advance notification on WLAN IC / FMAC driver hangup?
To output debug log, I suppose I have to define DEBUG and enable the definition of real brcmf_debugfs_fws_stats_read() which outputs multiple parameters.
If I managed to re-produce the hangup, which parameters to look for as general indication of hangup?
Best,
Wataru Sugimoto
Show LessHello,
I am in the process of upgrading to the 2019-05-03 release of the FMAC driver and I noticed today that this release is no longer available in the community site and that 2019-10-31 is now available.
Was it removed on purpose because it should not be used? Is 2019-05-03 safe to use or should I skip this release and use 2019-10-31 instead? I am using the Murata 1DX module (CYW4343W chipset).
Thanks,
Jesse
Show LessHi All,
We are working on NXP's imx8mq processor-based custom design. We have interfaced with the Murata's LBEE5HY1MW-230 module through the SDIO interface.
We used the 4.14 Linux distro for our development. This module's Wi-Fi and Bluetooth is working fine.
For the RF CE certification, we need to communicate with channel no 13.
For that, We configuring one router with channel no 13 with AP mode. Now we are trying to scan this SSID on our Murata's LBEE5HY1MW-230 module.
we are not able to connect the 13th channel of 2.4GHz band. It seems the country code issue with our firmware.
Can you please let us know where the changes are required to make connectivity with the 13th channel?
Please note there is no issue with connectivity up to the 11th channel.
Let me know if you need further information.
Thanks,
Parth
Show LessHi Experts,
We have purchased couple of CYW43455 modules and mounted on iMX7d 1GB board. I use Linux given by Toradex.
By default SDIO is not enabled and I don't see the WiFi up.
Could you please help me on this? whether to add any specific driver to make device up?
Thank You
Neeraj
Show LessI am trying to attach LM832 to my raspberry pi compute module. However i am not able to attach or find it. I think it will not require external drivers.
I am able to detect mmc1 as module. But on driver load I get
$ sudo modprobe brcmfmac
$ sudo dmesg -c
[ 381.903893] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 381.907147] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 381.939494] brcmfmac: F1 signature read @0x18000000=0x1541a9a6
[ 381.940215] brcmfmac: brcmf_chip_cores_check: CPU core not detected
[ 381.940229] brcmfmac: brcmf_sdio_probe_attach: brcmf_chip_attach failed!
[ 381.940249] brcmfmac: brcmf_sdio_probe: brcmf_sdio_probe_attach failed
[ 381.940518] brcmfmac: brcmf_ops_sdio_probe: F2 error, probe failed -19...
[ 381.940808] usbcore: registered new interface driver brcmfmac
What can be cause of such problem?
Show LessDear Community,
I have several questions. First, thank you for maintaining a helpful and knowledgeable community.
- Is this most up to date manual of the wl mfgtest utlility: CYW43XX Technical Information - WL Tool for Embedded 802.11 Systems ?
- Is there a batch/script file in the WICED SDK that outlines wl commands for evaluating spurious frequency
- My overall feedback is the wl tool needs more common scripts to assist customers with FCC 15C and CE-RED -- why do we need to reinvent the wheel?
- There are some example scripts/commands in WICED SDK (path: ./43xxx_Wi-Fi/libraries/test/wl_tool/scripts)
- I would like WICED community to share recent ARM 32/64 builds of the `wl` utility
- I am using kernel v4.19 and v5.3.y, prefer newer kernel
- I am evaluating two chipsets:
- BCM43430/CYW43430/CYW4343W
- BCM43438/CYW43438
- For those reading, you can find the mfgtest firmware for these chipsets in the WICED SDK (path: ./43xxx_Wi-Fi/resources/firmware/)
- Need util compiled for both architectures
- Can you attach to this thread, or shared on cypress github (Cypress Semiconductor Corporation · GitHub )
- These binaries need to be treated as a release -- perhaps you should bundle it with FMAC firmware releases?
Where is the official repository for up to date ARM binaries of the wl utility?
- For example you can find ARM builds here:
- Re: Check regulatory limit using curpower cmd : cmd failed
- Different hashes of this tool shouldn't live in forum posts
- What is the official position of Cypress/WICED community on wl builds from source code?
- Why not maintain these binaries in your github repo, similar to kernel/git/firmware/linux-firmware.git - Repository of firmware blobs for use with the Linux kernel
CC: Wi-Fi/Bluetooth for Linux and Android
Show LessI have a microcomputer running an embedded version of Linux 4.1.15-2.0.1. How do I use the wl utility in WLTEST mode?
Here's where I'm at right now:
root@XXXXXXXX:~# wl ver
1.107 RC5.0
wl0: Dec 29 2015 15:56:15 version 7.45.41.24 (r608913) FWID 01-4e412465
root@XXXXXXXX:~# ls /lib/firmware/bcm/
BCM43430A1.1DX.hcd bcmdhd.cal fw_bcmdhd.bin fw_bcmdhd_apsta.bin fw_bcmdhd_mfgtest.bin
root@XXXXXXXX:~#
What should I do next?
-Jason
Show LessHello,
I am evaluating the FMAC driver v4.14.77-2019_0503, as posted here: Cypress Linux WiFi Driver Release (FMAC) [2019-05-08]
Some of these patches do not apply to hostapd_2_7. Is there a version of the hostapd patches which would apply to that release? Or is hostapd_2_6 the only recommended version? I note that yocto "warrior" uses wpa_supplicant 2.7, and yocto "zeus" uses wpa_supplicant 2.9, so this is likely going to become a common question.
Many thanks for any assistance.
Show Less