Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Bluetooth for Linux Forum Discussions

AbhilashaD_26
Wi-Fi Bluetooth for Linux
Package Version ahd-2023_1221 Release Date 2023-12-21 Description Infineon Android release for the broad market. This release has been qualified on IM... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
Description The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version v5.15.58-2024_0118 Release Date 2024-01-18 Github Link V5.15.58 backport package: Link  V6.1.19 patch... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now. Description:  AIROC Bluetooth Stack is Infineon's Bluetooth Host Protoco... Show More
GauravS_31
Wi-Fi Bluetooth for Linux
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here: Sr. No. Driver release name Release link 1 Backports v5.15.58-2023_11... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version ahd-2022_1223 Release Date 2023-01-03 Description Cypress Android release for the broad market. This release has been qualified on Hik... Show More
hongkongkiwi
Wi-Fi Bluetooth for Linux
Hi there, We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor. We need help to compile the wl_tool... Show More
KrRa_4499631
Wi-Fi Bluetooth for Linux
Hi,I'm trying to setup a cyw43438 chip to run in station and AP mode simultaneously using wpa_supplicant and hostapd.I can successfully start an AP (s... Show More
DmAl_4630701
Wi-Fi Bluetooth for Linux
I spended so many time trying to understand, why WiFi module in rpi3b working only in G-mode (speed 54 Mb/s) and not N-mode.Tried many kernels, firmwa... Show More
MoRe_4591361
Wi-Fi Bluetooth for Linux
大家好,当我使用BCM43438设计了电路板后,我通过启动WL_REG_ON这个引脚,认为这个芯片应该已经正常工作了,测量各个电压也都很正确。可是当我测量晶振两端的电压时发现却没有任何电压,这是什么原因呢?我采用的似乎官方推荐的37.4MHz晶振和12pF电容。 Show More
KeTa_1341526
Wi-Fi Bluetooth for Linux
Hello,I am considering using the following FMAC driver.Cypress Linux WiFi Driver Release (FMAC) [2019-10-31] However, the Linux kernel version I want ... Show More
DiGh_4608241
Wi-Fi Bluetooth for Linux
Hello. I have recently come to know about the i.MX 8M Nano evk from NXP (i.MX 8M Nano Evaluation Kit | NXP ). It includes a Murata 1MW module, which I... Show More
DaFr_3582951
Wi-Fi Bluetooth for Linux
It seems that Cypress creates driver releases for the FMAC WiFi driver once in a while and the latest one (at the time of this post) is:Cypress Linux WiFi Driver Release (FMAC) [2019-10-31]... Show More
MiDi_4074381
Wi-Fi Bluetooth for Linux
Hello,I am using the Jody-W1 chip. I want to use all available channels in 5Ghz (that are allowed in current country). Unfortunately, the only frequen... Show More
owrp_4560236
Wi-Fi Bluetooth for Linux
Hi team,We use Cypress chip BCM43455 based Wi-FI+BT module with this we successfully up running wifi and BT.We are planning to go for regulation test.... Show More
owrp_4560236
Wi-Fi Bluetooth for Linux
Hello.We are trying to prepare Wi-Fi software test for the reference lab to certificate our device.( Linux machine)Our Communication Module uses a CYW... Show More
MIGO_1576536
Wi-Fi Bluetooth for Linux
Dear I am using CYW4343W (Murata LBEE5KL1DX) in our IMX6 Android8 platform.For FCC Certification we must be able to generate a Carrier into specific C... Show More