Wi-Fi Bluetooth for Linux Forum Discussions
Package Version
ahd-2023_1221
Release Date
2023-12-21
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform and Hikey960 PCIE platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* 4373-Android13-SDIO
*43012-Android13-SDIO
*43022-Android13-SDIO
*54591-Android13-PCIE
*55572-Android13-SDIO
*AHDBinaries
*device
*firmware
*nvram
* Android13_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
* confs
* hostapd_supplicant_src
* Android13_PCIE_Bringup.pdf
* Android13_SDIO_Bringup.pdf
* Android13_Feature_Bringup.pdf
Test Environment:
* IMX8 SDIO setup
* Hikey960 PCIE setup
* 55572, 43012, 43022, 54591 and 4373 Sanity, 6G and 11ax features (55572), WOWL via OOB(55572)
and PNO scan offload(55572, 43022)
Show LessDescription
The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code examples of Bluetooth® profiles) to evaluate and test Bluetooth® Classic and Low Energy on AIROC™ combo chip (CYW4373, CYW43439, CYW55573/2/1).
What's new?
Package comes with codes examples to demonstrate Bluetooth LE Audio capability of CYW55573/2/1 in hosted mode. The code example demonstrates Bluetooth® LE Audio unicast and broadcast functionality.
Functions include:
- Broadcast audio stream scanning
- Receiving broadcast audio stream
- Unicast audio stream establishment
- Unicast audio stream release
- Unicast sink connect to source (1 CIG, 1 CIS)
Bluetooth® Linux Code Examples & Supported Chip
Code example |
Feature demonstration |
Supported chip |
LE Audio CIS Source |
Implements the Unicast Source application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio CIS Sink |
Implements the Unicast Sink application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Source |
Demonstrates the ability of LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Sink |
Demonstrates the ability to receive LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® Find me |
Demonstrates the Find Me profile which defines the behavior when a button is pressed on one device to cause an alerting signal on a peer device |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® hello sensor |
Demonstrates GATT database and device configuration initialization, sending data to the client and processing write requests from the client |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Wi-Fi onboarding |
Demonstrates the feature that enables devices to connect to a Wi-Fi access point without requiring a physical interface |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Headset |
Multiple profile code example that demonstrates the use cases and ability of audio-related functions such as A2DP, AVRCP CT, and HFP |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® SPP |
Demonstrates how two devices can establish a wireless communication link that emulates a traditional serial port connection |
CYW43439,CYW4373 |
Package GitHub link: https://github.com/Infineon/ifx-linux-bluetooth
Release notes
Please go through the attached released notes for more details on the package.
Show Lessv5.15.58-2024_0118
Release Date
2024-01-18
Github Link
V5.15.58 backport package: Link
V6.1.19 patch: link
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
Part 1: cypress-fmac-v5.15.58-2023_1128.zip
* Backports package (cypress-backports-v5.15.58-2023_1128-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_1128.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_1128.tar.gz)
* Device tree files (cypress-devicetree-2023-11-28.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_1128.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Part 2: cypress-patch-v6.1.19-2023_1128.zip
* Cypress fmac patch files for Vanilla v6.1.19(cypress-patch-v6.1.19-2023_1128.tar.gz)
* Infineon-Vanilla-Kernel-v6.1.19-Bring-up-Reference_20201221.pdf
Checksum
cypress-fmac-v5.15.58-2023_1128 sha256sum:
990b5f6beeb9530525f254977569fd25936e09f9ef1bf36ca52118e73dff3e68 cypress-backports-v5.15.58-2023_1128-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
0c8da2efe289115f2242aa3f69de5bc616cb893ecd411e11194c4c008418bb2e cypress-custom-patch-5.4.21.tar.gz
c38cca05bb05db6198af7809c7a2e519cb33a06b02ebd4d626588c9038f7259b cypress-devicetree-2023-11-28.tar.gz
92608ceb4509cc02730833ce2119662b3c116a3956ca303245e97378186dc2a3 cypress-firmware-v5.15.58-2023_1128.tar.gz
771099830bd106307e77ebdd4d27a3e18de27bb60889c4db4bca81f44ade495d cypress-hostap_2_10-2023_1128.tar.gz
8fe7d8b677032fb04374615aae27c5a3131499956dc22ddb420847a3876974c6 cypress-patch-v5.15.58-2023_1128.tar.gz
cypress-patch-v6.1.19-2023_1128 sha256sum:
933ac3a50f0146b4078beb5e398c75a93ab0a1979a93d120a1c0ba2a06ab0ff7 Infineon-Kernel-v6.1.19-Bring-up-Reference.pdf
ac23fabed00e5c5ab0c3720fa0eb6fa135a589e009714f783701fe557abe3fe7 v6.1.19-2023_1128.tar.gz
Part 3: cypress-fmac-v5.15.58-2024_0118.zip
8ccbebf31bf69c85dc7d05fb7e3597fa282c3ba5373d76b2a65364191abb14d0 cypress-backports-v5.15.58-2024_0118-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
92e7196a896fa65138c8297d4202a1811564605360f807faa2c8af310eddeb2e cypress-custom-patch-5.4.21.tar.gz
40dd314cee28149028a2d524ccd5d25f20336c7314e1e26654daecf4c9a796d2 cypress-devicetree-2024-01-18.tar.gz
739d1fae54d885e136847af2957821324c18c68622f204992e268b991172da53 cypress-firmware-2024_0118.tar.gz
2a411fb64818b054498645f64e3ef3b29e4db9a36b65987d9a3af76c2d60f765 cypress-hostap_2_10-2024_0118.tar.gz
8e43bc4487c5d4e77880e2fc9d3152a011063c5b0f3871e277561f0108a88304 cypress-patch-v5.15.58-2024_0118.tar.gz
[Change Log]
2023-12-18 Initial Post
2023-12-22 Add cypress-patch-v6.1.19 to support build brcmfmac on 6.1.19
2024-01-18 Fix for system crash post suspend and resume with CYW55572/55573 [PCIe]
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now.
Description:
AIROC Bluetooth Stack is Infineon's Bluetooth Host Protocol Stack implementation. The stack is optimized to work with Infineon Bluetooth controllers. The BTSTACK supports Bluetooth BR/EDR and BLE core protocols. This page provides the Github links to get started with application developments in Linux platform using AIROC Bluetooth Stack.
Please find the code examples :
Code Examples:
https://github.com/Infineon/linux-example-btstack-wifi-onboarding
https://github.com/Infineon/linux-example-btstack-wakeonle
https://github.com/Infineon/linux-example-btstack-bas
https://github.com/Infineon/linux-example-btstack-hello-sensor
https://github.com/Infineon/linux-example-btstack-alert-client
https://github.com/Infineon/linux-example-btstack-alert-server
https://github.com/Infineon/linux-example-btstack-headset
https://github.com/Infineon/linux-example-btstack-a2dp-source
https://github.com/Infineon/linux-example-btstack-a2dp-sink
https://github.com/Infineon/linux-example-btstack-spp
https://github.com/Infineon/linux-example-btstack-handsfree-unit
https://github.com/Infineon/linux-example-btstack-handsfree-ag
Show Less
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here:
Sr. No. | Driver release name | Release link |
1 | Backports v5.15.58-2023_1128 |
Public forum link: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238 |
2 | 6.1 Latest kernel for RPI : RPI-6.1.21 IFXFMAC |
Github: https://github.com/Infineon/rpi-linux-kernel/releases/tag/6.1.21-hedorah-IFXFMAC-20231128 |
3 | 6.1 Kernel on BRCMFMAC |
Github: https://github.com/Infineon/ifx-wireless-drivers/tree/RTM/v6.1.19-hedorah |
Documentation is available in docs folder of cypress-fmac-v5.15.58-2023_1128.zip available at this link https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238
The older/archived Wi-Fi driver releases can be accessed here:
Show Less
Package Version
ahd-2022_1223
Release Date
2023-01-03
Description
Cypress Android release for the broad market.
This release has been qualified on Hikey 960 platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* ahd
* device
*hikey960
* firmware
* nvram
* 55572_AndroidBringup.pdf
Test Environment:
* Hikey 960
* 55572 Sanity and VTS
Change Log
[2022-12-23]
* Initial post
Show LessHi there,
We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor.
We need help to compile the wl_tool so we can proceed with certification, but we need it to be cross compiled for our architecture (arm 32bit).
Can I ask a representative to help us to compile it with our custom toolchain?
CPU Info:
- armv7l
- little-endian
- hard-float ABI
- neon/vfpv4
Custom Toolchain Instructions:
- download toolchain
- extract toolchain:
tar jxf arm-co6-linux-uclibcgnueabihf_sdk-buildroot_2021.02.1.tar.xz - cd to arm-co6-linux-uclibcgnueabihf_sdk-buildroot
- ./relocate_sdk.sh
- add toolchain into path e.g.
export PATH="$PATH:$PWD/usr/bin" - Set cross compile variables:
export ARCH=arm
export CROSS_COMPILE=arm-co6-linux-uclibcgnueabihf-
Tagging @VinayakS_26 / @raks_99 / @DoubleLo as I found they have helped another customer to do this.
Show Less
Package Version
v5.10.9-2021_1020
Release Date
2021-10-20
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.10.9-2021_1020-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.10.9-2021_1020.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.10.9-2021_1020.tar.gz)
* Device tree files (cypress-devicetree-2021-10-20.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-1-2021_1020.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum: 632ac3c28581d08ba91a083dd0edd60babb637274a6276b656435cdd298c57dd cypress-fmac-v5.10.9-2021_1020.zip 4241b4c636e5e4503ffc300481882dc69b64485cdf094105108e8a82d0b16797 cypress-backports-v5.10.9-2021_1020-module-src.tar.gz ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz 4aa347ba153ed4945737bf428fcee54877936998b5a60b16aa7cbbc87aaba7c6 cypress-devicetree-2021-10-20.tar.gz 95d2cb7c81c7fe60cc1811932b13f55ce5a9b4296f27182bfa57b3d37fe2a6f3 cypress-firmware-v5.10.9-2021_1020.tar.gz 88cce99e67f05c7bdfea8277740ad5bd06b54649c0b9c1dfc3052377b11f8091 cypress-hostap_2_9-1-2021_1020.tar.gz bdf37bb84ab5264dab09115df056182bf96fceff4792042d88bc66abc3058d08 cypress-patch-v5.10.9-2021_1020.tar.gz
[Change Log]
2021-10-26 Initial Post
Show LessPackage Version
v5.4.18-2021_0527
Release Date
2021-05-27
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.4.18-2021_0527-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.4.18-2021_0527.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.4.18-2021_0527.tar.gz)
* Device tree files (cypress-devicetree-2021-05-27.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-2021_0527.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum: 6dd1fe42791cb56fa4162d0a384cdca4052a428a259200afdc1eb2caa53543aa cypress-fmac-v5.4.18-2021_0527.zip 7b1f01076dc74fd1edf9983313822b9712d31a91bc4eb76e404fa37174c2bba0 cypress-backports-v5.4.18-2021_0527-module-src.tar.gz ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz 912598558111fcaa190e3dc319e53b91d1b84050af7e57dd3d2d5c889e856fa0 cypress-devicetree-2021-05-27.tar.gz 79698811c4a4756e9fd6bd0b26781f929b0b0405f24651efce07d805fe31c52d cypress-firmware-v5.4.18-2021_0527.tar.gz 63e3d9d0c7ed7182fae5e9ef55b1c99c5a907bac26f3959a6b8ae24d591a2c4f cypress-hostap_2_9-2021_0527.tar.gz 5302ec9679ec5af7e6a3b871fc06845468873cd2a55c381c7256af7eea647acf cypress-patch-v5.4.18-2021_0527.tar.gz
[Change Log]
2021-05-20 Initial Post
2021-05-27 Update documentation in doc/
2021-09-03 Firmware Update for 4356-pcie, 4339, 43362 (cypress-firmware-v5.4.18-2021_08_12.zip)
Show LessPackage Version
v5.4.18-2021_0114
Release Date
2021-01-21
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.4.18-2021_0114-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.4.18-2021_0114.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.4.18-2021_0114.tar.gz)
* Device tree files (cypress-devicetree-2021-01-21.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-2021_0114.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* README
Checksum
a3e914ed8e3b2e5057cdd3c6ab09ff2771a745bd767ba7aada33efe872b57899 cypress-fmac-v5.4.18-2021_0114.zip 17b987189e50fb539151e2931cf7deffe261a4c1e16a4ee4b08aca604480e03f cypress-backports-v5.4.18-2021_0114-module-src.tar.gz ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz 48a7f1a4935ac6286698d19149186c3b3ae11d0d68a2301e301fdfeeba453cb1 cypress-devicetree-2021-01-21.tar.gz c4bcfc14575a0d6a1954bc0c140eb2130ca8f2059194cee77b59e69fe7d0212d cypress-firmware-v5.4.18-2021_0114.tar.gz 074accc6e89882aaf3c3b05624f01d7669b64afab283e4d2ea33212791a5ea19 cypress-hostap_2_9-2021_0114.tar.gz 7cdee40e7df02718cea56d48358863eb6bd63c0ff641d82f5a5b566a66f644f7 cypress-patch-v5.4.18-2021_0114.tar.gz
Note
The same driver/firwmare is also released on GitHub. Here's the landing repo:
https://github.com/cypresssemiconductorco/ifx-linux-wireless
Change Log
[2021-03-05]
- Initial Post
Framework Version
cy-imx-android-10.0.0_2.0.0-6
Kernel Verison
Linux localhost 5.4.3-00002-ga85b5953f05b #1 SMP PREEMPT Wed Dec 23 07:58:53 CST 2020 aarch64
FMAC Version
v5.4.18-gamera-android-2-0-gde98449dbb46
Release Date
2021.01.22
Description
Cypress Android release for the broad market based on the NXP Android 10.0.0_2.0.0 release.
This release has been qualified on the NXP i.MX8MQuad Evaluation Kit (EVK) platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* backports-wireless
* cypress-fmac-patches
* firmware
* nvram
* aosp-patches
* utilities
* build.sh
* Cirrent Agent 1.50
* README
Test Environment
* ARM64 (NXP i.MX8MQuad Evaluation Kit)
* NXP Android 10.0.0_2.0.0
* 4354/45455/43012 Sanity and VTS
Change Log
[2021-03-05]
* Initial post
Show LessPackage Version
v5.4.18-2021_0114
Release Date
2021-01-21
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.4.18-2021_0114-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.4.18-2021_0114.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.4.18-2021_0114.tar.gz)
* Device tree files (cypress-devicetree-2021-01-21.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-2021_0114.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* README
Checksum
a3e914ed8e3b2e5057cdd3c6ab09ff2771a745bd767ba7aada33efe872b57899 cypress-fmac-v5.4.18-2021_0114.zip 17b987189e50fb539151e2931cf7deffe261a4c1e16a4ee4b08aca604480e03f cypress-backports-v5.4.18-2021_0114-module-src.tar.gz ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz 48a7f1a4935ac6286698d19149186c3b3ae11d0d68a2301e301fdfeeba453cb1 cypress-devicetree-2021-01-21.tar.gz c4bcfc14575a0d6a1954bc0c140eb2130ca8f2059194cee77b59e69fe7d0212d cypress-firmware-v5.4.18-2021_0114.tar.gz 074accc6e89882aaf3c3b05624f01d7669b64afab283e4d2ea33212791a5ea19 cypress-hostap_2_9-2021_0114.tar.gz 7cdee40e7df02718cea56d48358863eb6bd63c0ff641d82f5a5b566a66f644f7 cypress-patch-v5.4.18-2021_0114.tar.gz
Note
The same driver/firwmare is also released on GitHub. Here's the landing repo:
https://github.com/cypresssemiconductorco/ifx-linux-wireless
Change Log
[2021-03-05]
- Initial Post
Dear Cypress Infineon Linux Community,
In the Q2 2020 Software Release you may have noticed the device firmware for the 88x family has been removed. These parts are automotive industrial parts added into the commercial Linux software releases circa 2018 to provide an interim solution for the lack of a 2x2 MIMO industrial commercial portfolio offering. Effective Q1 2020 the 4373 (4373E industrial version coming soon) and 54591 commercial parts are now available and the 88x products for commercial designs have been transitioned to NRND (Not Recommended for New Designs). As such, the Q2 2020 software release for Linux removed 88x devices. Customers are encouraged to leverage the 4373 or 54591 for future commercial designs. Customers with existing (commercial) investment in the 88x product families may rest easy as these parts REMAIN UNDER PRODUCT MAINTENANCE AND WILL CONTINUE TO BE SUPPORTED with bug fix firmware + driver releases (including any critical CVE remediation) on a case by case basis. The Q3 A-Class Technical Brief will be posted at the end of September and will contain additional information information about this and other device life cycle changes planned for the upcoming year.
To use this this firmware, simply drop these firmware files into your fmac's "firmware" folder. The latest fmac driver code has not removed support for the CYW88x devices, so a simple copy/paste will get you up and running with the latest driver and these binaries.
There have been no changes to this firmware since the q1 2020 release. No changes to this firmware are currently planned. This posting is aimed to provide software continuity for customers with in-flight designs on 88x families.
This posting will be updated in the future with future software/firmware assets that are moved into the MAINTENANCE state. Customers are encouraged to read the Commercial Software Lifecycle chapter in the Connectivity Solutions for Linux and Android Technical Brief for more information about the Software Lifecycle.
Show LessHi,
I put together the steps it took me to use this relatively new package Cypress Linux WiFi Driver Release (FMAC) [2019-05-08]
You can find all the details / steps here:
https://dokuwiki.alu4u.com/doku.php?id=stellar-wireless-wpa3-sae-raspberry-pi
Thanks,
Regards,
Benny
Show LessFYI: Linux is a joy . For those who might have issues with the CYW43907AEVAL1F being recognized as two ttyUSB ports, this might be helpful.
Background: Things were working fine with my Linux Mint 19 PC, though there is a console fonts issue (another story not yet resolved).
I reinstalled Linux Mint 19 on my PC. After the reinstall, the FTDI FT2232H USB chip was not visible on /dev/ttyUSB0/1 anymore. I entered "dmesg" to see that "Broadcom" was recognized, but no serial ports.
I did find a workaround as follows (with help from https://ubuntuforums.org/showthread.php?t=2259068 😞
1. Enter:
sudo modprobe ftdi_sio idVendor=0x0a5c idProduct=0x43fa
(When I plug in the board, I see via the command "dmesg":
New USB device found, idVendor=0a5c, idProduct=43fa, bcdDevice= 7.00)
2. Enter (per the recommended workaround, above):
sudo chmod 666 /sys/bus/usb-serial/drivers/ftdi_sio/new_id
3. Use a text editor to edit a new file:
/sys/bus/usb-serial/drivers/ftdi_sio/new_id
Add only these two numbers to the file (i.e., the idVendor and idProduct):
0x0a5c 0x43fa
Then save it.
4. Enter (if not already done, I think this needs to be done only once):
sudo usermod -a -G dialout your_user_name
5. Plug in the board, and verify:
dmesg | grep tty
You should see something like:
[ 45.511352] usb 2-2: FTDI USB Serial Device converter now attached to ttyUSB0
[ 45.511672] usb 2-2: FTDI USB Serial Device converter now attached to ttyUSB1
Now, I need to do this after each reboot since the file "new_id" does not appear to be saved.
I use the serial program "moserial" to connect to ttyUSB1, and I can see serial activity now.
I might need to unplug/plug in the board if download fails.
Whew.
I hope this helps someone out there.
Show LessADB shell 파일 첨부 함.
- « Previous
-
- 1
- 2
- Next »