Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Bluetooth for Linux Forum Discussions

AbhilashaD_26
Wi-Fi Bluetooth for Linux
Package Version ahd-2023_1221 Release Date 2023-12-21 Description Infineon Android release for the broad market. This release has been qualified on IM... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
Description The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version v5.15.58-2024_0118 Release Date 2024-01-18 Github Link V5.15.58 backport package: Link  V6.1.19 patch... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now. Description:  AIROC Bluetooth Stack is Infineon's Bluetooth Host Protoco... Show More
GauravS_31
Wi-Fi Bluetooth for Linux
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here: Sr. No. Driver release name Release link 1 Backports v5.15.58-2023_11... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version ahd-2022_1223 Release Date 2023-01-03 Description Cypress Android release for the broad market. This release has been qualified on Hik... Show More
hongkongkiwi
Wi-Fi Bluetooth for Linux
Hi there, We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor. We need help to compile the wl_tool... Show More
srme_3928751
Wi-Fi Bluetooth for Linux
Hi,  I have an BCM4355 chip interfaced to SM32MP157 processor,both the drivers for WIFI/BLE are loading.But while running any operation on them I am f... Show More
JeKh_2254986
Wi-Fi Bluetooth for Linux
We are connecting CYW88359  W-Lan + BLE module on our set top box to BCM7628 PCIe interface via a PCIe switch instead of directly to the SoC as we nee... Show More
jach_2064941
Wi-Fi Bluetooth for Linux
hi Is CYW89359 workable under NXP i.MX8QM Xen and OS Android™ P9.0.0_2.1.0-AUTO-ga james Show More
ApNa_2097886
Wi-Fi Bluetooth for Linux
Hi ,We recently tried to upgrade our 4.14.77 backports fmac driver to the latest 5.4.18 backports version.The 4.14.77 backports was also being run on ... Show More
SLa_4731906
Wi-Fi Bluetooth for Linux
Hi all,  Our device we are working with v4.14.34-backports. Now recently I am trying to upgrade the driver using v5.4.18-backports drop. I get the fol... Show More
RaRa_4733311
Wi-Fi Bluetooth for Linux
Hi,Since our board BSP is based on Linux 4.9, we need an appropriate compatible sdio driver.These are some steps we tried so far :Downloaded and Backp... Show More
JoPr_4729106
Wi-Fi Bluetooth for Linux
Hi please can you provide the Preliminary Data Sheet for CYW4360 / BCM4360 chip? I cannot find it anywhere. Thank you Show More
EdTy_2191711
Wi-Fi Bluetooth for Linux
Hi,Our product is unable to connect to WiFi channels 12 and higher. Out build is using the 1DX with v5.4.18-2020_0402 firmware and the latest Linux ke... Show More
raji_4720746
Wi-Fi Bluetooth for Linux
Hi everyone:    I am porting wifi module on my customed-board with imx8Quad chip,the board I am using is highly similar to imx8QuadXPlus. The wifi mod... Show More
Leo_liu1
Wi-Fi Bluetooth for Linux
Hi Sir,Hi Sir,我用的平台是IMX6 ,LINUX环境,DHD driver,CYW43438运行在STA 模式。目前考虑到功耗问题,想要通过调节DTIM的值,改变监听的间隔,从而达到省电的目的,但是在DHD driver里面改了一些参数,没有起到作用,也尝试通过wl dtim命令设置,... Show More