Package Version
v5.10.9-2022_0511
Release Date
2022-05-11
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.10.9-2022_0511-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.10.9-2022_0511.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.10.9-2022_0511.tar.gz)
* Device tree files (cypress-devicetree-2022-05-13.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-1-2022_0511.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum:
7cf529c371f0bc8c47908c42359879aee308970b34e7c5e971bd9a79124f215b cypress-backports-v5.10.9-2022_0511-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
4bce8d957b451f7d9a23bd77121eea920bde372f6097424c6e87d6a61aa34d9e cypress-devicetree-2022-05-13.tar.gz
8b301a0828f4eecfc261039bff01a875edc0f93c58887814941b7cdfbe8bacb8 cypress-firmware-v5.10.9-2022_0511.tar.gz
ca748efbef2b6197a50152e3d51fb028949be5bbcb2474b67e2e35dd5aa1804f cypress-hostap_2_9-1-2022_0511.tar.gz
8201ad2e8720279f5baf870be57fe15be49d714bcaa0653c0faa8de80b8a2c51 cypress-patch-v5.10.9-2022_0511.tar.gz
ec1311ceddd80e3a24dbf2976cbbfbb043d7909d8cd91c4254da563d3dedf9e8 README.txt
[Change Log]
2022-06-07 Initial Post
Show LessHi there,
We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor.
We need help to compile the wl_tool so we can proceed with certification, but we need it to be cross compiled for our architecture (arm 32bit).
Can I ask a representative to help us to compile it with our custom toolchain?
CPU Info:
Custom Toolchain Instructions:
Tagging @VinayakS_26 / @raks_99 / @DoubleLo as I found they have helped another customer to do this.
Show Less
Hello,
We are using a CYW43455 on Android 11, linux kernel 5.10.72 (NXP BSP)
The bring-up went OK with brcmfmac driver and wpa_supplicant. We are now able to use the wlan interfrace.
However the Compatibility Test Suite (CTS) reveals that we don't have a proper Wifi HAL. There used to be a specific HAL for bcmdhd driver, but this driver has been removed from recent kernels.
Is there a recommended wifi HAL for brcmfmac driver ?
Best regards,
For emissions testing, I am trying to use the wl tool with NVIDA Jetson TX2, which has the BCM4354. I received a wl64 executable and 4354’s mfgtest firmware from an Infineon Tech Support Case.
I believe I correctly installed the mfgtest firmware by replacing /lib/firmware/brcm/fw_bcmdhd.bin with cyfmac4354-sdio.bin and by moving cyfmac4354-sdio.clm_blob to become /lib/firmware/brcm/bcmdhd.clm_blob. Before the above changes, running “sudo ./wl64 ver” gave me:
1.28 RC0.0
wl0: Jul 21 2020 16:35:45 version 7.35.349.94 (r726700 CY) FWID 01-aa356e32
After installing mfgtest firmware, the wl ver command gave me:
1.28 RC0.0
wl0: Sep 1 2021 02:23:00 version 7.35.349.112 (ae8cc29 CY WLTEST) FWID 01-6e1af42a
My main problem is that wl64 can’t bring up the Wi-Fi after I use it to bring down the Wi-Fi. It also doesn't work using the original firmware (i.e., before introducing the mfgtest firmware). The following are the commands I ran and the output.
user@device:~$ ip -br address show wlan0
wlan0 UP 192.168.0.79/24
user@device:~$ sudo ./wl64 down
user@device:~$ ip -br address show wlan0
wlan0 DORMANT 192.168.0.79/24
(after ~20 seconds)
user@device:~$ ip -br address show wlan0
wlan0 DORMANT
user@device:~$ sudo ./wl64 up
user@device:~$ ip -br address show wlan0
wlan0 DORMANT
At this point, I also can’t use the GUI to connect to a Wi-FI network.
Have I done anything wrong? What do I do so that I can at least use the wl tool to bring down and up the Wi-Fi module?
Show Less
Hi @AnjanaM_61
I cannot give reply over there (above link) so continuing my question here.
As by your answer (3rd point), other options for HFP and A2DP were Linux or Android. So, both the chipsets CYW4343W and CYW43012 support HFP and A2DP. So, kindly send me the links of respective SDKs, so that I can evaluate and finalize the chipset for our application.
And please be noted that, in Linux and Android SDKs must contain A2DP, HFP and HSP supporting SBC and AAC codecs.
Thanks and Regards.
Vinayak
Show Less
My setup:
- ARM host processor running 5.10 Linux.
- Murata 1MW BT/Wi-Fi combo chip (BCM43455) over SDIO
- Wi-Fi firmware: version 7.45.249
- Using linux/hostapd patch sets from "cypress-fmac-v5.10.9-2022_0511"
The issue:
After removing the brcmfmac kernel module, Bluetooth performs very poorly (drops active connections, scan no longer detects devices, sco audio is extremely crackly if the connection does not drop, etc.). This is only observed if Wi-Fi was associated to an AP within 3 seconds of kernel module removal. Re-inserting the module always corrects the issue.
- Start with brcmfmac modules loaded and associated to an AP, then run the following in a script:
ifdown wlan0
modprobe -r brcmfmac
- Bluetooth performs poorly
- Start with brcmfmac modules loaded and associated to an AP, then run the following in a script:
wpa_cli disconnect
sleep 3
ifdown wlan0
modprobe -r brcmfmac
- Bluetooth functions normally.
Once I realized a 3 second delay after disconnect prevented the issue, I investigated to see how late in the module removal the delay could be placed before the issue began to occur again. I tried moving the delay into the kernel module itself and found that as long as the 3 second delay is put before the call to brcm_chip_set_passive() made in brcmf_sdio_remove(), then the issue is avoided. If I place it after that call, then I experience the poor Bluetooth performance.
It seems like the module is left in a state where Bluetooth is in low priority. Perhaps the module is still attempting to disassociate with the network when the chip is placed in passive mode? I am trying to understand what is happening so that I can avoid this issue properly, rather than inserting a long delay and hoping it is always sufficient.
Any insight as to what is happening would be greatly appreciated. It is difficult to find information on the BT/Wi-Fi coexistence mechanism used by this chip.
Thank you,
Show LessPackage Version
v5.10.9-2022_0511
Release Date
2022-05-11
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.10.9-2022_0511-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.10.9-2022_0511.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.10.9-2022_0511.tar.gz)
* Device tree files (cypress-devicetree-2022-05-13.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-1-2022_0511.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum:
7cf529c371f0bc8c47908c42359879aee308970b34e7c5e971bd9a79124f215b cypress-backports-v5.10.9-2022_0511-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
4bce8d957b451f7d9a23bd77121eea920bde372f6097424c6e87d6a61aa34d9e cypress-devicetree-2022-05-13.tar.gz
8b301a0828f4eecfc261039bff01a875edc0f93c58887814941b7cdfbe8bacb8 cypress-firmware-v5.10.9-2022_0511.tar.gz
ca748efbef2b6197a50152e3d51fb028949be5bbcb2474b67e2e35dd5aa1804f cypress-hostap_2_9-1-2022_0511.tar.gz
8201ad2e8720279f5baf870be57fe15be49d714bcaa0653c0faa8de80b8a2c51 cypress-patch-v5.10.9-2022_0511.tar.gz
ec1311ceddd80e3a24dbf2976cbbfbb043d7909d8cd91c4254da563d3dedf9e8 README.txt
[Change Log]
2022-06-07 Initial Post
Show LessHi All,
We are using CYW43012 chipset and recently moved from:
Firmware version:
1.21 RC0.0
wl0: Sep 1 2021 22:33:32 version 13.10.271.273 (9278a67 CY) FWID 01-e6c8687a
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
to
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v5.10.9-2022_0321-0-ga0971bc0b123
We found that the DFS channel support for US country is currently disabled in the latest release where as it was working in the older release.
Old release:
root@SAMA5D2C3:~# wl ver
1.21 RC0.0
wl0: Dec 13 2019 03:35:44 version 13.10.271.227 (6ca6a80) FWID 01-396d897 tws:GENR.3.1.2
root@SAMA5D2C3:~# wl country
US (US/0) UNITED STATES
root@SAMA5D2C3:~# wl channels
36 40 44 48 52 56 60 64 100 104 108 112 116 120 124 128 132 136 140 144 149 153 157 161 165
root@SAMA5D2C3:~# wl chan_info
Channel 36 A Band
Channel 40 A Band
Channel 44 A Band
Channel 48 A Band
Channel 52 A Band, RADAR Sensitive
Channel 56 A Band, RADAR Sensitive
Channel 60 A Band, RADAR Sensitive
Channel 64 A Band, RADAR Sensitive
Channel 100 A Band, RADAR Sensitive
Channel 104 A Band, RADAR Sensitive
Channel 108 A Band, RADAR Sensitive
Channel 112 A Band, RADAR Sensitive
Channel 116 A Band, RADAR Sensitive
Channel 120 A Band, RADAR Sensitive
Channel 124 A Band, RADAR Sensitive
Channel 128 A Band, RADAR Sensitive
Channel 132 A Band, RADAR Sensitive
Channel 136 A Band, RADAR Sensitive
Channel 140 A Band, RADAR Sensitive
Channel 144 A Band, RADAR Sensitive
Channel 149 A Band
Channel 153 A Band
Channel 157 A Band
Channel 161 A Band
Channel 165 A Band
root@SAMA5D2C3:~#
New Release:
root@SAMA5D2C3:/etc/broadcom/wifi# wl country
US (US/0) UNITED STATES
root@SAMA5D2C3:/etc/broadcom/wifi# wl channels
36 40 44 48 149 153 157 161 165
root@SAMA5D2C3:/etc/broadcom/wifi# wl chan_info
Channel 36 A Band
Channel 40 A Band
Channel 44 A Band
Channel 48 A Band
Channel 149 A Band
Channel 153 A Band
Channel 157 A Band
Channel 161 A Band
Channel 165 A Band
Using the old clm_blob file is working fine with the new release. Can you please let us know how to reenable DFS channels and any other parameters in the new release?
Regards,
Rupesh
Show LessHi All,
We are using CYW43012 chipset and recently moved from:
Firmware version:
1.21 RC0.0
wl0: Sep 1 2021 22:33:32 version 13.10.271.273 (9278a67 CY) FWID 01-e6c8687a
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
to
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v5.10.9-2022_0321-0-ga0971bc0b123
We are seeing increase in power consumption by 20mA approximately after we upgrade the release.
We have observed that only by changing the driver the power consumption increases but not with the firmware upgrade.
We couldn't figure out what exactly caused increase in the power cosumption.
Can someone help us figure out the reason for the same as our product is an battery powered embedded device which makes it very critical for us.
Please let me know if you need any information.
Regards,
Rupesh
Show LessHi All,
We are using CYW43012 chipset with the following details:
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
We have observed that after certain time, we are seeing SDIO -110 error as follows:
2022-05-04 02:44:53 SAMA5D2C3 kernel:[45542.850000] +++ should not come 470:atmel_i2s_switch_mck_generator
2022-05-04 02:45:01 SAMA5D2C3 crond[699]: pam_unix(crond:session): session opened for user root by (uid=0)
2022-05-04 02:45:01 SAMA5D2C3 CROND[700]: (root) CMD (/bin/date -u +%4Y%2m%2d%2H%2M%2S 2>/dev/null > /etc/timestamp)
2022-05-04 02:45:01 SAMA5D2C3 CROND[699]: pam_unix(crond:session): session closed for user root
2022-05-04 02:46:09 SAMA5D2C3 rsyslogd: -- MARK --
2022-05-04 02:46:15 SAMA5D2C3 kernel:[45624.750000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:46:58 SAMA5D2C3 kernel:[45667.480000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:48:58 SAMA5D2C3 kernel:[45787.500000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.300000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.320000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.330000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.350000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.360000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.370000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.390000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.400000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.420000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.440000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.440000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.560000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.570000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.580000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.700000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.720000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.730000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.950000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.960000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.980000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F0@0x00003, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.990000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.010000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.020000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.040000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.050000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.070000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.080000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.100000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.110000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.120000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.140000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.160000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.170000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.190000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.200000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.220000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.220000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.240000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.260000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.270000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.290000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.300000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.320000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.340000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.340000] brcmfmac: brcmf_sdio_dpc: sdio ctrlframe tx failed err=-110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.350000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.360000] brcmfmac: brcmf_proto_bcdc_query_dcmd: brcmf_proto_bcdc_msg failed w/status -110
This issue is frequently reproducible and any need asap is deeply appreciated.
Attached the complete log file for your reference.
Regards,
Rupesh
Show LessHello,
As part of the industrialization of a project, I want to pass the compule module 4 card in a certification laboratory.
I developed a distribution using yocto. I am looking for an application that allows the wifi module of the compute module 4 to be transmitted.
I need to make the module transmit at 2.4GHz at the minimum, center and maximum frequency.
I have to do the same with both frequencies in 5GHz. (minimum, central and maximum)
Do you have an ARM application and commands that allow me to do this?
Thank a lot.
Arthur
Show Less
User | Count |
---|---|
4 | |
3 | |
3 | |
2 |