Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Bluetooth for Linux Forum Discussions

AbhilashaD_26
Wi-Fi Bluetooth for Linux
Package Version ahd-2023_1221 Release Date 2023-12-21 Description Infineon Android release for the broad market. This release has been qualified on IM... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
Description The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version v5.15.58-2024_0118 Release Date 2024-01-18 Github Link V5.15.58 backport package: Link  V6.1.19 patch... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now. Description:  AIROC Bluetooth Stack is Infineon's Bluetooth Host Protoco... Show More
GauravS_31
Wi-Fi Bluetooth for Linux
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here: Sr. No. Driver release name Release link 1 Backports v5.15.58-2023_11... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version ahd-2022_1223 Release Date 2023-01-03 Description Cypress Android release for the broad market. This release has been qualified on Hik... Show More
hongkongkiwi
Wi-Fi Bluetooth for Linux
Hi there, We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor. We need help to compile the wl_tool... Show More
user_4848521
Wi-Fi Bluetooth for Linux
Does the driver brcm43430 / cyfmac43430 support setting bitrates with iw?I'm getting the following error when trying to force valid bitrates for a var... Show More
MichaelF_56
Wi-Fi Bluetooth for Linux
I'm excited to let the Infineon developer community know that Murata’s own support community is now up and running at https://community.murata.com/s/ ... Show More
JuCh_4848291
Wi-Fi Bluetooth for Linux
Trying to add WPA3 for BCM4359, but wpa_supplicant will fail to start if ieee80211w was set to 1 or 2. We suspect the driver we have may not have PMF ... Show More
Leo_Liu
Wi-Fi Bluetooth for Linux
Hi SIr,目前在评估43455在AP模式下的自动选择信道的功能,DHD driver是否支持DFS以及ACS功能,我在driver有看到wl_support_ACS的宏,是否Makefile打开这个宏就可以支持ACS?关于DFS的功能是否支持,如何验证呢,谢谢 Show More
BaM_4840156
Wi-Fi Bluetooth for Linux
Hi Folks,AnjanaM_61​ I’m using CYM43455 module with the customized board and Jetson Xavier NX SoM. When I try to pair bluetooth with other bluetooth s... Show More
YoTa_1693656
Wi-Fi Bluetooth for Linux
Hello, Infineon/Cypress team[Issue]We are evaluating below FMAC driver below to use CYW43455. The FMAC driver occurs memory leak.https://community.cypress.com/docs/DOC-21490... Show More
AjKu_4703686
Wi-Fi Bluetooth for Linux
Hi Team,I added the CYW43455 WIFI/BT chip support in the Jetson Platform using the following driver/firmware Cypress Linux WiFi Driver Release (FMAC) [2020-09-25]... Show More
BaM_4840156
Wi-Fi Bluetooth for Linux
Hi Team,I’m using CYM43455 module with the customized board and Jetson Xavier NX SoM.When I try to do hciattach command, first few times the command i... Show More
PeHa_4793326
Wi-Fi Bluetooth for Linux
I'm trying to test the cyfmac54591 module with an NVIDIA Jetson Nano, and running into an issue with loading FW during 'insmod brcmfmac.ko' :from dmes... Show More
paPr_4835046
Wi-Fi Bluetooth for Linux
Hi  our team has to build sama5d3_xplained based board currently we are stuck in the wifi+bt section. we are using the "Cypress CYW4343W" chipset bel... Show More