Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Bluetooth for Linux Forum Discussions

AbhilashaD_26
Wi-Fi Bluetooth for Linux
Package Version ahd-2023_1221 Release Date 2023-12-21 Description Infineon Android release for the broad market. This release has been qualified on IM... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
Description The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version v5.15.58-2024_0118 Release Date 2024-01-18 Github Link V5.15.58 backport package: Link  V6.1.19 patch... Show More
AnjanaM_61
Wi-Fi Bluetooth for Linux
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now. Description:  AIROC Bluetooth Stack is Infineon's Bluetooth Host Protoco... Show More
GauravS_31
Wi-Fi Bluetooth for Linux
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here: Sr. No. Driver release name Release link 1 Backports v5.15.58-2023_11... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version ahd-2022_1223 Release Date 2023-01-03 Description Cypress Android release for the broad market. This release has been qualified on Hik... Show More
hongkongkiwi
Wi-Fi Bluetooth for Linux
Hi there, We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor. We need help to compile the wl_tool... Show More
JoDi_3981251
Wi-Fi Bluetooth for Linux
Hi , We are using CYW43455 chip as WIFI STA. We find this module can't discover the AP which is set to WPA2 TKIP only. So, I want to check whether thi... Show More
marcin
Wi-Fi Bluetooth for Linux
Hi! I'm representing Conclusive Engineering we are creating a custom board that utilizes CYW4343WKUBG chip for WiFi and Bluetooth connections. Based ... Show More
Leo_Liu
Wi-Fi Bluetooth for Linux
Hi Sir, 我在调试43455的时候,在加载FW出现error,导致DHD 加载失败。 我使用的环境是IMX.8的平台,arm64,Linux4.18,DHD版本125.15~125.19都有验证过,海华197(43438),288(43362),256(43455)EVK,其中197,288都... Show More
JeHa_4771251
Wi-Fi Bluetooth for Linux
Hello,  We have custom board with a 43012 connected via SDIO to a Xilinx ZynqMP.    We are using the latest Xilinx release which run the 5.4.0 kernel.... Show More
JiSh_4749101
Wi-Fi Bluetooth for Linux
Hi, I'm  I followed the instuctions on page 3 of WICED™ Manufacturing Test User Guide   Now I have a problem when I enter the command to "sudo ./wl -i... Show More
deepanr
Wi-Fi Bluetooth for Linux
Hi , We are integrated CYW89820BWMLGT BT module along with our imx6 based processor. So we wanted to program the module with the BT stack. Can you ple... Show More
AjKu_4703686
Wi-Fi Bluetooth for Linux
Hi Team,1) Does the CYW43455 chip support ad-hoc mode in WIFI?2) Is there any procedure/command-line tools available to set up an ad-hoc network using... Show More
jues_4844976
Wi-Fi Bluetooth for Linux
Hi, where can I find the most recent version of wl_tool ? I have downloaded the one from this post but it seems to not integrate all the commands (phy... Show More
lida_4439816
Wi-Fi Bluetooth for Linux
hi everyone:     when i compiling the backports package,there is a question:lex -ozconf.lex.c -L zconf.lyacc -ozconf.tab.c -t -l zconf.yyacc: e - line... Show More
MaRa_4792956
Wi-Fi Bluetooth for Linux
Hardware details,   Cypress Chipset              Default Options           WLAN Interface          Devices Supported  =============             ======... Show More