Wi-Fi Bluetooth for Linux Forum Discussions
Package Version
ahd-2023_1221
Release Date
2023-12-21
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform and Hikey960 PCIE platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* 4373-Android13-SDIO
*43012-Android13-SDIO
*43022-Android13-SDIO
*54591-Android13-PCIE
*55572-Android13-SDIO
*AHDBinaries
*device
*firmware
*nvram
* Android13_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
* confs
* hostapd_supplicant_src
* Android13_PCIE_Bringup.pdf
* Android13_SDIO_Bringup.pdf
* Android13_Feature_Bringup.pdf
Test Environment:
* IMX8 SDIO setup
* Hikey960 PCIE setup
* 55572, 43012, 43022, 54591 and 4373 Sanity, 6G and 11ax features (55572), WOWL via OOB(55572)
and PNO scan offload(55572, 43022)
Show LessDescription
The package contains all the required files (including AIROC™ Bluetooth® stack for ARMv8 Linux, Bluetooth® porting layer, and sample code examples of Bluetooth® profiles) to evaluate and test Bluetooth® Classic and Low Energy on AIROC™ combo chip (CYW4373, CYW43439, CYW55573/2/1).
What's new?
Package comes with codes examples to demonstrate Bluetooth LE Audio capability of CYW55573/2/1 in hosted mode. The code example demonstrates Bluetooth® LE Audio unicast and broadcast functionality.
Functions include:
- Broadcast audio stream scanning
- Receiving broadcast audio stream
- Unicast audio stream establishment
- Unicast audio stream release
- Unicast sink connect to source (1 CIG, 1 CIS)
Bluetooth® Linux Code Examples & Supported Chip
Code example |
Feature demonstration |
Supported chip |
LE Audio CIS Source |
Implements the Unicast Source application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio CIS Sink |
Implements the Unicast Sink application using BTSTACK and LE-Audio profile library |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Source |
Demonstrates the ability of LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
LE Audio BIS Sink |
Demonstrates the ability to receive LE Audio broadcast |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® Find me |
Demonstrates the Find Me profile which defines the behavior when a button is pressed on one device to cause an alerting signal on a peer device |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® hello sensor |
Demonstrates GATT database and device configuration initialization, sending data to the client and processing write requests from the client |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Wi-Fi onboarding |
Demonstrates the feature that enables devices to connect to a Wi-Fi access point without requiring a physical interface |
CYW55573/CYW55572/CYW55571 CYW43439,CYW4373 |
Linux Bluetooth® Headset |
Multiple profile code example that demonstrates the use cases and ability of audio-related functions such as A2DP, AVRCP CT, and HFP |
CYW55573/CYW55572/CYW55571 |
Linux Bluetooth® SPP |
Demonstrates how two devices can establish a wireless communication link that emulates a traditional serial port connection |
CYW43439,CYW4373 |
Package GitHub link: https://github.com/Infineon/ifx-linux-bluetooth
Release notes
Please go through the attached released notes for more details on the package.
Show Lessv5.15.58-2024_0118
Release Date
2024-01-18
Github Link
V5.15.58 backport package: Link
V6.1.19 patch: link
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
Part 1: cypress-fmac-v5.15.58-2023_1128.zip
* Backports package (cypress-backports-v5.15.58-2023_1128-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_1128.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_1128.tar.gz)
* Device tree files (cypress-devicetree-2023-11-28.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_1128.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Part 2: cypress-patch-v6.1.19-2023_1128.zip
* Cypress fmac patch files for Vanilla v6.1.19(cypress-patch-v6.1.19-2023_1128.tar.gz)
* Infineon-Vanilla-Kernel-v6.1.19-Bring-up-Reference_20201221.pdf
Checksum
cypress-fmac-v5.15.58-2023_1128 sha256sum:
990b5f6beeb9530525f254977569fd25936e09f9ef1bf36ca52118e73dff3e68 cypress-backports-v5.15.58-2023_1128-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
0c8da2efe289115f2242aa3f69de5bc616cb893ecd411e11194c4c008418bb2e cypress-custom-patch-5.4.21.tar.gz
c38cca05bb05db6198af7809c7a2e519cb33a06b02ebd4d626588c9038f7259b cypress-devicetree-2023-11-28.tar.gz
92608ceb4509cc02730833ce2119662b3c116a3956ca303245e97378186dc2a3 cypress-firmware-v5.15.58-2023_1128.tar.gz
771099830bd106307e77ebdd4d27a3e18de27bb60889c4db4bca81f44ade495d cypress-hostap_2_10-2023_1128.tar.gz
8fe7d8b677032fb04374615aae27c5a3131499956dc22ddb420847a3876974c6 cypress-patch-v5.15.58-2023_1128.tar.gz
cypress-patch-v6.1.19-2023_1128 sha256sum:
933ac3a50f0146b4078beb5e398c75a93ab0a1979a93d120a1c0ba2a06ab0ff7 Infineon-Kernel-v6.1.19-Bring-up-Reference.pdf
ac23fabed00e5c5ab0c3720fa0eb6fa135a589e009714f783701fe557abe3fe7 v6.1.19-2023_1128.tar.gz
Part 3: cypress-fmac-v5.15.58-2024_0118.zip
8ccbebf31bf69c85dc7d05fb7e3597fa282c3ba5373d76b2a65364191abb14d0 cypress-backports-v5.15.58-2024_0118-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
92e7196a896fa65138c8297d4202a1811564605360f807faa2c8af310eddeb2e cypress-custom-patch-5.4.21.tar.gz
40dd314cee28149028a2d524ccd5d25f20336c7314e1e26654daecf4c9a796d2 cypress-devicetree-2024-01-18.tar.gz
739d1fae54d885e136847af2957821324c18c68622f204992e268b991172da53 cypress-firmware-2024_0118.tar.gz
2a411fb64818b054498645f64e3ef3b29e4db9a36b65987d9a3af76c2d60f765 cypress-hostap_2_10-2024_0118.tar.gz
8e43bc4487c5d4e77880e2fc9d3152a011063c5b0f3871e277561f0108a88304 cypress-patch-v5.15.58-2024_0118.tar.gz
[Change Log]
2023-12-18 Initial Post
2023-12-22 Add cypress-patch-v6.1.19 to support build brcmfmac on 6.1.19
2024-01-18 Fix for system crash post suspend and resume with CYW55572/55573 [PCIe]
The BT assets of AIROC Bluetooth Stack (Linux) Release are all on GitHub now.
Description:
AIROC Bluetooth Stack is Infineon's Bluetooth Host Protocol Stack implementation. The stack is optimized to work with Infineon Bluetooth controllers. The BTSTACK supports Bluetooth BR/EDR and BLE core protocols. This page provides the Github links to get started with application developments in Linux platform using AIROC Bluetooth Stack.
Please find the code examples :
Code Examples:
https://github.com/Infineon/linux-example-btstack-wifi-onboarding
https://github.com/Infineon/linux-example-btstack-wakeonle
https://github.com/Infineon/linux-example-btstack-bas
https://github.com/Infineon/linux-example-btstack-hello-sensor
https://github.com/Infineon/linux-example-btstack-alert-client
https://github.com/Infineon/linux-example-btstack-alert-server
https://github.com/Infineon/linux-example-btstack-headset
https://github.com/Infineon/linux-example-btstack-a2dp-source
https://github.com/Infineon/linux-example-btstack-a2dp-sink
https://github.com/Infineon/linux-example-btstack-spp
https://github.com/Infineon/linux-example-btstack-handsfree-unit
https://github.com/Infineon/linux-example-btstack-handsfree-ag
Show Less
The latest Infineon Linux Wi-Fi driver (FMAC) release can be accessed here:
Sr. No. | Driver release name | Release link |
1 | Backports v5.15.58-2023_1128 |
Public forum link: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238 |
2 | 6.1 Latest kernel for RPI : RPI-6.1.21 IFXFMAC |
Github: https://github.com/Infineon/rpi-linux-kernel/releases/tag/6.1.21-hedorah-IFXFMAC-20231128 |
3 | 6.1 Kernel on BRCMFMAC |
Github: https://github.com/Infineon/ifx-wireless-drivers/tree/RTM/v6.1.19-hedorah |
Documentation is available in docs folder of cypress-fmac-v5.15.58-2023_1128.zip available at this link https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-11-28/td-p/662238
The older/archived Wi-Fi driver releases can be accessed here:
Show Less
Package Version
ahd-2022_1223
Release Date
2023-01-03
Description
Cypress Android release for the broad market.
This release has been qualified on Hikey 960 platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* ahd
* device
*hikey960
* firmware
* nvram
* 55572_AndroidBringup.pdf
Test Environment:
* Hikey 960
* 55572 Sanity and VTS
Change Log
[2022-12-23]
* Initial post
Show LessHi there,
We are trying to fcc wifi certify our project which uses a custom buildroot toolchain and arm processor.
We need help to compile the wl_tool so we can proceed with certification, but we need it to be cross compiled for our architecture (arm 32bit).
Can I ask a representative to help us to compile it with our custom toolchain?
CPU Info:
- armv7l
- little-endian
- hard-float ABI
- neon/vfpv4
Custom Toolchain Instructions:
- download toolchain
- extract toolchain:
tar jxf arm-co6-linux-uclibcgnueabihf_sdk-buildroot_2021.02.1.tar.xz - cd to arm-co6-linux-uclibcgnueabihf_sdk-buildroot
- ./relocate_sdk.sh
- add toolchain into path e.g.
export PATH="$PATH:$PWD/usr/bin" - Set cross compile variables:
export ARCH=arm
export CROSS_COMPILE=arm-co6-linux-uclibcgnueabihf-
Tagging @VinayakS_26 / @raks_99 / @DoubleLo as I found they have helped another customer to do this.
Show Less
We are using the CYW43012 (LBEE591LV Module) for Bluetooth in slave PCM mode not i2S mode in order to replace a now obsolete module. Therefore the CLK, DATA_IN and SYNC are all inputs to the module / chipset.
What clock edge should the data, and sync signals be sampled on please as the PCM Interface Timing Diagrams were removed in the CYW43012 datasheet (document number 002-18925 Rev *J). Does anybody know why? Is this interface / protocol not supported / not working and do we have to use the i2S configuration instead?
Show LessHi All,
We are using CYW43012 chipset and recently moved from:
Firmware version:
1.21 RC0.0
wl0: Sep 1 2021 22:33:32 version 13.10.271.273 (9278a67 CY) FWID 01-e6c8687a
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
to
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v5.10.9-2022_0321-0-ga0971bc0b123
We are seeing increase in power consumption by 20mA approximately after we upgrade the release.
We have observed that only by changing the driver the power consumption increases but not with the firmware upgrade.
We couldn't figure out what exactly caused increase in the power cosumption.
Can someone help us figure out the reason for the same as our product is an battery powered embedded device which makes it very critical for us.
Please let me know if you need any information.
Regards,
Rupesh
Show LessHello,
As part of the industrialization of a project, I want to pass the compule module 4 card in a certification laboratory.
I developed a distribution using yocto. I am looking for an application that allows the wifi module of the compute module 4 to be transmitted.
I need to make the module transmit at 2.4GHz at the minimum, center and maximum frequency.
I have to do the same with both frequencies in 5GHz. (minimum, central and maximum)
Do you have an ARM application and commands that allow me to do this?
Thank a lot.
Arthur
Show Less
Hello,
We are using a CYW43455 on Android 11, linux kernel 5.10.72 (NXP BSP)
The bring-up went OK with brcmfmac driver and wpa_supplicant. We are now able to use the wlan interfrace.
However the Compatibility Test Suite (CTS) reveals that we don't have a proper Wifi HAL. There used to be a specific HAL for bcmdhd driver, but this driver has been removed from recent kernels.
Is there a recommended wifi HAL for brcmfmac driver ?
Best regards,
Hi @AnjanaM_61
I cannot give reply over there (above link) so continuing my question here.
As by your answer (3rd point), other options for HFP and A2DP were Linux or Android. So, both the chipsets CYW4343W and CYW43012 support HFP and A2DP. So, kindly send me the links of respective SDKs, so that I can evaluate and finalize the chipset for our application.
And please be noted that, in Linux and Android SDKs must contain A2DP, HFP and HSP supporting SBC and AAC codecs.
Thanks and Regards.
Vinayak
Show Less
Hi All,
We are using CYW43012 chipset and recently moved from:
Firmware version:
1.21 RC0.0
wl0: Sep 1 2021 22:33:32 version 13.10.271.273 (9278a67 CY) FWID 01-e6c8687a
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
to
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v5.10.9-2022_0321-0-ga0971bc0b123
We found that the DFS channel support for US country is currently disabled in the latest release where as it was working in the older release.
Old release:
root@SAMA5D2C3:~# wl ver
1.21 RC0.0
wl0: Dec 13 2019 03:35:44 version 13.10.271.227 (6ca6a80) FWID 01-396d897 tws:GENR.3.1.2
root@SAMA5D2C3:~# wl country
US (US/0) UNITED STATES
root@SAMA5D2C3:~# wl channels
36 40 44 48 52 56 60 64 100 104 108 112 116 120 124 128 132 136 140 144 149 153 157 161 165
root@SAMA5D2C3:~# wl chan_info
Channel 36 A Band
Channel 40 A Band
Channel 44 A Band
Channel 48 A Band
Channel 52 A Band, RADAR Sensitive
Channel 56 A Band, RADAR Sensitive
Channel 60 A Band, RADAR Sensitive
Channel 64 A Band, RADAR Sensitive
Channel 100 A Band, RADAR Sensitive
Channel 104 A Band, RADAR Sensitive
Channel 108 A Band, RADAR Sensitive
Channel 112 A Band, RADAR Sensitive
Channel 116 A Band, RADAR Sensitive
Channel 120 A Band, RADAR Sensitive
Channel 124 A Band, RADAR Sensitive
Channel 128 A Band, RADAR Sensitive
Channel 132 A Band, RADAR Sensitive
Channel 136 A Band, RADAR Sensitive
Channel 140 A Band, RADAR Sensitive
Channel 144 A Band, RADAR Sensitive
Channel 149 A Band
Channel 153 A Band
Channel 157 A Band
Channel 161 A Band
Channel 165 A Band
root@SAMA5D2C3:~#
New Release:
root@SAMA5D2C3:/etc/broadcom/wifi# wl country
US (US/0) UNITED STATES
root@SAMA5D2C3:/etc/broadcom/wifi# wl channels
36 40 44 48 149 153 157 161 165
root@SAMA5D2C3:/etc/broadcom/wifi# wl chan_info
Channel 36 A Band
Channel 40 A Band
Channel 44 A Band
Channel 48 A Band
Channel 149 A Band
Channel 153 A Band
Channel 157 A Band
Channel 161 A Band
Channel 165 A Band
Using the old clm_blob file is working fine with the new release. Can you please let us know how to reenable DFS channels and any other parameters in the new release?
Regards,
Rupesh
Show LessHi All,
We are using CYW43012 chipset with the following details:
Firmware version:
1.21 RC0.0
wl0: Feb 21 2022 07:19:28 version 13.10.271.283 (211da63 CY) FWID 01-18f4ac2
Driver Version:
Backported Linux Version v4.14.77-kong-RTM-rc8-0-ged6fa18
We have observed that after certain time, we are seeing SDIO -110 error as follows:
2022-05-04 02:44:53 SAMA5D2C3 kernel:[45542.850000] +++ should not come 470:atmel_i2s_switch_mck_generator
2022-05-04 02:45:01 SAMA5D2C3 crond[699]: pam_unix(crond:session): session opened for user root by (uid=0)
2022-05-04 02:45:01 SAMA5D2C3 CROND[700]: (root) CMD (/bin/date -u +%4Y%2m%2d%2H%2M%2S 2>/dev/null > /etc/timestamp)
2022-05-04 02:45:01 SAMA5D2C3 CROND[699]: pam_unix(crond:session): session closed for user root
2022-05-04 02:46:09 SAMA5D2C3 rsyslogd: -- MARK --
2022-05-04 02:46:15 SAMA5D2C3 kernel:[45624.750000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:46:58 SAMA5D2C3 kernel:[45667.480000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:48:58 SAMA5D2C3 kernel:[45787.500000] atmel_i2s f8050000.i2s: TX underrun on channel 0
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.300000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.320000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.330000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.350000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.360000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.370000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.390000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.400000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.420000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.440000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.440000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.560000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.570000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.580000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.700000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.720000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.730000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.950000] brcmfmac: brcmf_sdio_bus_sleep: error while changing bus sleep state -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.960000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x0a020, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.980000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F0@0x00003, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45809.990000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.010000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.020000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.040000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.050000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.070000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.080000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.100000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.110000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.120000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.140000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.160000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.170000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.190000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.200000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.220000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:20 SAMA5D2C3 kernel:[45810.220000] brcmfmac: brcmf_sdio_txfail: sdio error, abort command and terminate frame
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.240000] brcmfmac: brcmf_sdiod_regrw_helper: failed to write data F1@0x1000d, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.260000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.270000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.290000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.300000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.320000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x1001a, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.340000] brcmfmac: brcmf_sdiod_regrw_helper: failed to read data F1@0x10019, err: -110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.340000] brcmfmac: brcmf_sdio_dpc: sdio ctrlframe tx failed err=-110
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.350000] brcmfmac: brcmf_sdio_dpc: failed backplane access over SDIO, halting operation
2022-05-04 02:49:21 SAMA5D2C3 kernel:[45810.360000] brcmfmac: brcmf_proto_bcdc_query_dcmd: brcmf_proto_bcdc_msg failed w/status -110
This issue is frequently reproducible and any need asap is deeply appreciated.
Attached the complete log file for your reference.
Regards,
Rupesh
Show LessHi Cypress Team,
We need to do Pre-compliance tests on CYW43455 module on Android 11 platform for WiFi and BT.
Could you please provide us any tools(like WL and HCITOOL in linux) to do the same for Android 11.
Also, could you provide us relevant documentation for the same.
Thanks.
Show Less