Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Bluetooth for Linux Forum Discussions

divyeshmarne
Level 1
First reply posted First question asked Welcome!
Level 1

Hi Team,

We have integrated CYW43444 module with android and everything working properly.

We have to do RF testing for WIFI.

We have WL binary.. 

But We are getting error for somw commands. Can you please help here.

evk_8mm:/ # wl pkteng_start 00:11:22:33:44:55 tx sync 40 1000 0
wl: error -23

evk_8mm:/ # wl country ALL
wl: error -2

evk_8mm:/ # wl phy_watchdog 0
wl: error -23

Requirement :

  1. Transmit in continuous wave mode.
  2. Transmit in Packet mode (No of Packets configurable).
  3. Transmit in continuous stream (duty cycle more than 90%).
  4. Receive in packet and continuous mode (Time configurable).

What needs to be done for above requirement? 

Also following commands are not working:

divyeshmarne_0-1659095979597.png

10 wl country ALL
11 wl dump
12 wl pkteng_start 00:11:22:33:44:55 tx 20 1500 0
13 wl pkteng_stats
14 wl nvram_dump

 

Thanks

Divyesh

0 Likes
5 Replies
GauravS_31
Moderator
Moderator 250 sign-ins First comment on KBA 5 questions asked
Moderator

You will require WLAN mfgtest firmware to test pkteng.

0 Likes
divyeshmarne
Level 1
First reply posted First question asked Welcome!
Level 1

Hi @GauravS_31 ,

Could you please provide firmware for the same

Module : CYW43455 1MW.  

Please provide the complete details for it.

Thanks

Divyesh

0 Likes
MuraliR_36
Moderator
Moderator 250 sign-ins 250 replies posted 100 solutions authored
Moderator

PFA the mfgtest firmware.

0 Likes
divyeshmarne
Level 1
First reply posted First question asked Welcome!
Level 1

Hi @MuraliR_36 ,

We have few firmware files pushed in device :

divyeshmarne_0-1659418863989.png

So apart from this, do I need to push file which you have shared just now?

What to keep file for this?

 

 

0 Likes
MuraliR_36
Moderator
Moderator 250 sign-ins 250 replies posted 100 solutions authored
Moderator

replace the brcmfmac43455-sdio.bin with the .bin file I shared and reload the drivers.

The file name should be the same.

0 Likes