- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Team,
We have integrated CYW43444 module with android and everything working properly.
We have to do RF testing for WIFI.
We have WL binary..
But We are getting error for somw commands. Can you please help here.
evk_8mm:/ # wl pkteng_start 00:11:22:33:44:55 tx sync 40 1000 0
wl: error -23
evk_8mm:/ # wl country ALL
wl: error -2
evk_8mm:/ # wl phy_watchdog 0
wl: error -23
Requirement :
- Transmit in continuous wave mode.
- Transmit in Packet mode (No of Packets configurable).
- Transmit in continuous stream (duty cycle more than 90%).
- Receive in packet and continuous mode (Time configurable).
What needs to be done for above requirement?
Also following commands are not working:
10 wl country ALL
11 wl dump
12 wl pkteng_start 00:11:22:33:44:55 tx 20 1500 0
13 wl pkteng_stats
14 wl nvram_dump
Thanks
Divyesh
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
You will require WLAN mfgtest firmware to test pkteng.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @GauravS_31 ,
Could you please provide firmware for the same
Module : CYW43455 1MW.
Please provide the complete details for it.
Thanks
Divyesh
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
Hi @Murali_R ,
We have few firmware files pushed in device :
So apart from this, do I need to push file which you have shared just now?
What to keep file for this?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
replace the brcmfmac43455-sdio.bin with the .bin file I shared and reload the drivers.
The file name should be the same.