Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Where can I find the WL utility for the CYW4354?  I need an ARM64 Linux version.  Is there any hope of finding this?

   -Dennis

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.

Hi Dennis,

I have compiled wl source for arm64 as well as x86 64 architectures.The toolchain that you have mentioned earlier was

linaro-5.3-2016.02-x86_64_aarch64-linux-gnu

which is for x86 64bit architecture.

PFA the required files. hope this works for you.

View solution in original post

7 Replies
VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

Hi,

Could you provide the toolchain that you are using. Is it arm-none-gnu-eabi.gcc ? if this is the case, then we could compile the source with the appropriate toolchain an give you the utility.

0 Likes
Anonymous
Not applicable

Hi Dennis,

Can you please tell us your toolchain.

BR,

Aman

0 Likes
Anonymous
Not applicable

My toolchain is linaro-5.3-2016.02-x86_64_aarch64-linux-gnu

  -Dennis Millard

  -Tealdrones

MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

The 4354 is not a broad marker device that's supported within WICED, nor am I aware of any partners that build modules with this device.  Could you provide the partner name as well. It make make more sense for you to work through the local sales team that enabled you on this device to line up the appropriate factory support.

Anonymous
Not applicable

We are using the BCM4354 (CYW4354) which is built-in to the nVidia TX1

SOM.  We have talked to nVidia for support and finally their internal

team suggested we go to Cypress for support.  At this point the chip

manufacturer and the module manufacturer are pointing fingers at each

other, and we've got no support.

If we could just get the WLAN Client Utility compiled for ARM64, then

maybe we can figure things out ourselves.

  -Dennis Millard

lock attach
Attachments are accessible only for community members.

Hi Dennis,

I have compiled wl source for arm64 as well as x86 64 architectures.The toolchain that you have mentioned earlier was

linaro-5.3-2016.02-x86_64_aarch64-linux-gnu

which is for x86 64bit architecture.

PFA the required files. hope this works for you.

Anonymous
Not applicable

We are in the same boat as the OP. Thanks for sharing the command line tool!

Would you be kind enough to also share the manufacturer firmware and nvram binary, so we can use it with the command line tool? We have scheduled our EMC test, your immediate assistant will be very much appreciated! Thank you!

0 Likes