cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Bluetooth for Linux

ew
New Contributor II

Hi

I'm using your latests brcmfmac firmware (released 15.Jan.2020),

with a Murata 1MW module with 43455 chipset.

The platform I'm using is a iMX6 with Linux kernel 5.4 & hostapd version 2.9.

WPA2 is working fine already, but for WPA3 I'm missing an example

hostap.conf, which was succesfuly tested by Cypress !

Please provide a good example of this configuration file,

tested with an iPhone with current iOS 13, ideally 🙂

Thanks

ew

1 Solution
VinayakS_26
Moderator
Moderator

Hi,

PFA a sample hostapd.conf file with wpa3 support.

Make sure to enable CONFIG_SAE=y aand CONFIG_IEEE80211N=y in your .config file while building the hostapd source.

Regards

View solution in original post

0 Likes
2 Replies
VinayakS_26
Moderator
Moderator

Hi,

PFA a sample hostapd.conf file with wpa3 support.

Make sure to enable CONFIG_SAE=y aand CONFIG_IEEE80211N=y in your .config file while building the hostapd source.

Regards

View solution in original post

0 Likes
yasa_4608926
Contributor II

Hi,

I am also using it. (cypress-fmac-v4.14.77-2020_0115.zip)

The following parameters are set in hostapd.conf for WPA3, and it's working fine.

ieee80211w=2

wpa_key_mgmt=SAE

rsn_pairwise=CCMP

sae_password=<password>

Best regards,

Yasa