Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Bluetooth for Linux Forum Discussions

zzzz_4377811
Level 2
Level 2
5 replies posted 10 questions asked Welcome!

hello:

In the following two paths for wiced 6.4:

paths 1:43xxx_wifi/platforms/BCM943340WCD1/wifi_nvram.h

paths 2:43xxx_wifi/platforms/BCM943362WCD4/wifi_nvram.h

The following two parameters are different:

    "edonthd=-65"                                                        "\x00"

    "edoffthd=-71"                                                       "\x00"

Path 1 doesn't exist. Path 2 does

I want to know the meaning of these two parameters and their impact on wifi usage,thinks!

0 Likes
1 Solution
Zhengbao_Zhang
Moderator
Moderator
Moderator
First comment on KBA 10 questions asked 5 questions asked

Hello :

We also often used below command to trigger Adaptivity test.

So your command showed in the nv table, means the active range is from -65 to -71.

wl phy_ed_thresh -70

This command is to adjust the Energy Detect (Adaptivity) sensitivity level. Range is

from -20 to -75, but never below -75

View solution in original post

0 Likes
1 Reply
Zhengbao_Zhang
Moderator
Moderator
Moderator
First comment on KBA 10 questions asked 5 questions asked

Hello :

We also often used below command to trigger Adaptivity test.

So your command showed in the nv table, means the active range is from -65 to -71.

wl phy_ed_thresh -70

This command is to adjust the Energy Detect (Adaptivity) sensitivity level. Range is

from -20 to -75, but never below -75

0 Likes