Device rebooting due to brcm crash

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Hrithik
Level 3
Level 3
25 sign-ins 25 replies posted First solution authored

Hi Infineon Team,

We are using CYW43455 chip for WiFi BT and our SoC is iMX8M Mini working on Android 11OS.
Sometimes, the device is getting reboot with below dmesg crash logs:

Internal error: Oops: 96000004 [#1] PREEMPT SMP
Modules linked in: brcmfmac brcmutil synaptics_dsx_i2c
CPU: 3 PID: 675 Comm: wpa_supplicant Tainted: G W 5.10.35-gc94a7dbc06b3 #1
Hardware name: FSL i.MX8MM DDR4 EVK with CYW43455 WIFI/BT board (DT)
pstate: 80400005 (Nzcv daif +PAN -UAO -TCO BTYPE=--)
pc : brcmf_p2p_tx_action_frame+0x80/0x188 [brcmfmac]
lr : brcmf_p2p_send_action_frame+0x3c4/0x63c [brcmfmac]
sp : ffff80001d8c36b0
x29: ffff80001d8c36b0 x28: 0000000000000000
x27: ffff0000ca45c820 x26: 00000000ffff029b
x25: 00000000000003e8 x24: ffff0000ca45c820
x23: ffff0000ca134818 x22: ffff00001aafe000
x21: ffff00001aafe000 x20: ffff0000ca134900
x19: ffff0000ca134810 x18: ffff80001d335098
x17: 000000000000aec2 x16: 00000000000009ff
x15: 0000000000000000 x14: 0000000000001400
x13: 0000000000000004 x12: 000000000698d000
x11: 0000000000000000 x10: 0000000000000000
x9 : 0000000000000038 x8 : 0000000000000000
x7 : 0000000000000000 x6 : 0005a7d5b2f6639e
x5 : 00000000efe4b99a x4 : 0000000000000001
x3 : 0000000000000724 x2 : ffff00001aafe000
x1 : ffff8000096067ff x0 : ffff0000ca134810
Call trace:
brcmf_p2p_tx_action_frame+0x80/0x188 [brcmfmac]
brcmf_p2p_send_action_frame+0x3c4/0x63c [brcmfmac]
brcmf_cfg80211_mgmt_tx+0x1d4/0x28c [brcmfmac]
rdev_mgmt_tx+0x3c/0x184
cfg80211_mlme_mgmt_tx+0x1c8/0x270
nl80211_tx_mgmt+0x1f8/0x32c
genl_rcv_msg+0x38c/0x3b8
netlink_rcv_skb+0x108/0x124
genl_rcv+0x38/0x54
netlink_unicast_kernel+0xa0/0x138
netlink_unicast+0xfc/0x1a0
netlink_sendmsg+0x284/0x314
____sys_sendmsg+0x170/0x228
__sys_sendmsg+0x11c/0x180
__arm64_sys_sendmsg+0x28/0x38
el0_svc_common+0xa4/0x180
do_el0_svc+0x28/0x7c
el0_svc+0x14/0x24
el0_sync_handler+0x6c/0xb4
el0_sync+0x19c/0x1c0
Code: 9a890108 f8686a68 5280e483 aa1503e2 (f9400100)
---[ end trace 2aa4f42fdd3f96b2 ]---
Kernel panic - not syncing: Oops: Fatal exception

Please find the attached complete logs for reference.
Could you kindly let me know what the issue could be?

Thanks.

0 Likes
1 Solution
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

closing the issue due to inactivity.

View solution in original post

0 Likes
5 Replies
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

Hi @Hrithik , Looks like you are using an older version of the driver will check and get back to you on the logs

0 Likes
Hrithik
Level 3
Level 3
25 sign-ins 25 replies posted First solution authored

Hi @Vivek_gunapati ,

Did you find the cause of brcm crash from the logs?

Thanks.

0 Likes

Hi @Hrithik , As i understand that you are porting and upgrading the driver to a newer release. 
Could you please let us know if the driver crashes with the newer release as well?

Regards
Vivek.

0 Likes

Hi @Hrithik since you would be using the ported driver could we close this issue?

0 Likes
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

closing the issue due to inactivity.

0 Likes