Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Bluetooth for Linux Forum Discussions

DoubleLo
Employee
Employee
50 sign-ins 10 questions asked First reply posted
Package Version

v5.15.58-2023_0222

Release Date

2023-02-21

Description

This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.

Files in this release:
* Backports package (cypress-backports-v5.15.58-2023_0222-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_0222.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_0222.tar.gz)
* Device tree files (cypress-devicetree-2023-02-21.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_0222.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README

Checksum

sha256sum:
c4498f5905726efbcd0f434a3f981bb1a2516edbea3723f3e9ddebde5a4fd16a cypress-backports-v5.15.58-2023_0222-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
7a5606cf3637873cfab0aa852f56eab9ca9ce5d537761c4b149503210607f500 cypress-devicetree-2023-02-21.tar.gz
416c68f74d835678c61244a12e12a22ccf340394f1f61ca7f5cb69c261686a03 cypress-firmware-v5.15.58-2023_0222.tar.gz
ca3679140d11885411b66db2438a143fa3015d41a1ae22268f1b097070b1d48f cypress-hostap_2_10-2023_0222.tar.gz
0894cb2c6afa24cd829f662925fd65f2650770be7bb5d4c271d33c2a2474b285 cypress-patch-v5.15.58-2023_0222.tar.gz

 [Change Log]

2023-02-23 Initial Post

 

4 Replies
kkk
Level 1
Level 1
First question asked First reply posted Welcome!

Thanks, while you are at it, please fix the directory rights in the tarballs and provide direct links to the single tarballs.

By the way:

https://community.infineon.com/gfawx74859/attachments/gfawx74859/WiFiBluetoothLinux/2685/2/cypress-f...

This file is not a gzipped tarball but a zip file. Hopefully you can fix this too.

 

0 Likes
Vivek_gunapati
Moderator
Moderator
Moderator
First question asked 5 likes given 250 sign-ins

Hi @kkk

In the current release 43455 and 4354 firmware did not make it to this release. It should be available in the next release. 

Regards
Vivek.

0 Likes
kkk
Level 1
Level 1
First question asked First reply posted Welcome!

Thank you for your response.

So your documentation in this release about the support for CYW43455 is misleading, right? I was hoping to know if there are any estimates on when the next release will be available.

Ultimately, my goal (and I guess that of most customers) is to have all necessary components supported in the mainline kernel, so we can avoid relying on your vague schedule. Is there any progress or plan towards having mailine support without vendor patches?

For any further projects, I will make sure to prioritize hardware that has first-class Linux kernel mainline support to avoid having to rely on vendor patching. The additional work required to support proprietary patches is quite burdensome. I'm telling you this to motivate, not criticize.

Additionally, I'm wondering if there is anything we can do to help speed up the process. Would it be beneficial if someone from our corporate or FAE team reaches out to the relevant parties?

Thank you for your time and assistance

PS: Also, I noticed that our last question was censored. Can you please clarify why that was the case and re-establish the thread so that we can all see the progress? Transparency and open communication are important to us and we want to ensure that we are all on the same page.

0 Likes
NoraMorin
Level 1
Level 1
First reply posted Welcome!

Thanks for the answer.

0 Likes
This widget could not be displayed.