Cypress Linux WiFi Driver Release (FMAC) [2022-09-09]

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
DoubleLo
Employee
Employee
50 sign-ins 10 questions asked First reply posted

Package Version

v5.10.9-2022_0909

Release Date

2022-09-14

Description

This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.

Files in this release:
* Backports package (cypress-backports-v5.10.9-2022_0909-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.10.9-2022_0909.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.10.9-2022_0909.tar.gz)
* Device tree files (cypress-devicetree-2022-09-12.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2022_0909.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README

Checksum

 

sha256sum: 
6d96b39c39871d98912639f0ffd55cfbe2e7fd86f3928cb111b6c832bd57d7af  cypress-fmac-v5.10.9-2022_0909.zip
0da7f2694a2764ed5ccc094aa101c0b0f47fb728eaaadce47380589e669589eb  cypress-backports-v5.10.9-2022_0909-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55  cypress-cirrent-1.60.tar.gz
e013c426c718b629aa1c1b580e5c55a61577443ed7e98179d29c05970514e8b9  cypress-devicetree-2022-09-12.tar.gz
7f8a20aa83f36e8fe59d8c4535ff5a16882a6d71fc93719ab91a23ee45e855f7  cypress-firmware-v5.10.9-2022_0909.tar.gz
d27939550b3522f864ef032c7fa50e3f5da9555070885bc069d4fb17aaa34f68  cypress-hostap_2_10-2022_0909.tar.gz
790b2d0115df5fbd2a537a9294da7c18a0b4a7b5a7a10fbfc78c0000772e75ce  cypress-patch-v5.10.9-2022_0909.tar.gz

 

 

 [Change Log]

2022-09-14 Initial Post

0 Likes
5 Replies
user_ah
Level 4
Level 4
Distributor - Avnet(GC)
5 solutions authored 25 replies posted 100 sign-ins

Hi,

Dose this version support CYW54591 and CYW55572 WiFi with SDIO interface??

Austin

0 Likes

Hi @user_ah  , Yes, cyfmac54591-sdio.bin & cyfmac55572-sdio.trxse are part of the firmware folder in the above package.

0 Likes
mfwitten
Level 1
Level 1
First reply posted Welcome!

Perhaps, work with Arend van Spriel on this patch series:

Specifically, this patch may be of interest to you:

Certainly, it is untenable to remain pursuing the current approach of maintaining a list of patches atop increasingly ancient source code. Please be actual engineers, and craft something properly.

0 Likes
Lavanya
Level 3
Level 3
25 sign-ins 5 questions asked 10 replies posted

Hi Does this release support 43455? I could not see the list of supported chipset in the README file

0 Likes
Lavanya
Level 3
Level 3
25 sign-ins 5 questions asked 10 replies posted

I went through the lists for firmware binaries I do see cyfmac43455-sdio.bin available in the firmware so I got my answer thanks.