Download the new Linux Driver

Download Now

Wi-Fi Bluetooth for Linux

Chi-HsienL_21
Employee
10 likes received 10 questions asked 10 sign-ins
Employee

Package Version

v5.4.18-2021_0114

Release Date

2021-01-21

Description

This is Cypress's Linux brcmfmac driver and firmware support package.

Brcmfmac is an open-source driver project.

Files in this release:
* Backports package (cypress-backports-v5.4.18-2021_0114-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.4.18-2021_0114.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.4.18-2021_0114.tar.gz)
* Device tree files (cypress-devicetree-2021-01-21.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-2021_0114.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* README

Checksum

a3e914ed8e3b2e5057cdd3c6ab09ff2771a745bd767ba7aada33efe872b57899  cypress-fmac-v5.4.18-2021_0114.zip
17b987189e50fb539151e2931cf7deffe261a4c1e16a4ee4b08aca604480e03f  cypress-backports-v5.4.18-2021_0114-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55  cypress-cirrent-1.60.tar.gz
48a7f1a4935ac6286698d19149186c3b3ae11d0d68a2301e301fdfeeba453cb1  cypress-devicetree-2021-01-21.tar.gz
c4bcfc14575a0d6a1954bc0c140eb2130ca8f2059194cee77b59e69fe7d0212d  cypress-firmware-v5.4.18-2021_0114.tar.gz
074accc6e89882aaf3c3b05624f01d7669b64afab283e4d2ea33212791a5ea19  cypress-hostap_2_9-2021_0114.tar.gz
7cdee40e7df02718cea56d48358863eb6bd63c0ff641d82f5a5b566a66f644f7  cypress-patch-v5.4.18-2021_0114.tar.gz

Note

The same driver/firwmare is also released on GitHub. Here's the landing repo:

https://github.com/cypresssemiconductorco/ifx-linux-wireless

Change Log

[2021-03-05]

  1. Initial Post
0 Likes
0 Replies