- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi everyone, I am trying to use bcm43438 on linux, and the wifi is working well. But when i use Bluez on linux to test the bluetooth, it doesn't work.
Firstly i use command 'hciattach /dev/ttymxc2 bcm43xx 3000000 flow -t 10' to init the device, but it will get time out, then I digged into the process, and I found the command will call function bcm43xx_init:
``````
int bcm43xx_init(int fd, int def_speed, int speed, struct termios *ti,
const char *bdaddr)
{
char chip_name[20];
char fw_path[PATH_MAX];
printf("bcm43xx_init\n");
if (bcm43xx_reset(fd))
return -1;
printf("reset successfully\n"); //whether program can get here
if (bcm43xx_read_local_name(fd, chip_name, sizeof(chip_name)))
return -1;
printf("read local name successfully\n"); //whether program can get here
if (bcm43xx_locate_patch(FIRMWARE_DIR, chip_name, fw_path)) {
fprintf(stderr, "Patch not found, continue anyway\n");
} else {
if (bcm43xx_set_speed(fd, ti, speed))
return -1;
if (bcm43xx_load_firmware(fd, fw_path))
return -1;
.....
`````````````````````
I add two 'printf' to indicate where is wrong, and the result shows it can reset successfully then get time out. So it gets time out in bcm43xx_read_local_name, the code is like this:
````````````````````````
static int bcm43xx_read_local_name(int fd, char *name, size_t size)
{
unsigned char cmd[] = { HCI_COMMAND_PKT, 0x14, 0x0C, 0x00 };
unsigned char *resp;
unsigned int name_len;
resp = malloc(size + CC_MIN_SIZE);
if (!resp)
return -1;
tcflush(fd, TCIOFLUSH);
if (write(fd, cmd, sizeof(cmd)) != sizeof(cmd)) {
fprintf(stderr, "Failed to write read local name command\n");
goto fail;
}
// it is stucked here
if (read_hci_event(fd, resp, size) < CC_MIN_SIZE) {
fprintf(stderr, "Failed to read local name, invalid HCI event\n");
goto fail;
}
if (resp[4] != cmd[1] || resp[5] != cmd[2] || resp[6] != CMD_SUCCESS) {
fprintf(stderr, "Failed to read local name, command failure\n");
goto fail;
}
`````
After I tried many times, I found it is stucked in read_hci_event function, the host can not get response from device. But it can get response in bcm43xx_reset(), so i think it is the problem of hci command, then i changed the hci command many times, it turned out the device only response to the reset hci command. I don't know why is it so.
The Bluez version is 5.37 and the linux kernel is 4.1.38.
Please give me some advice, thanks very much.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
try hciattach /dev/ttymxc2 bcm43xx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Which partner and partner module are you working with?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
try hciattach /dev/ttymxc2 bcm43xx