Announcements

Community will be in read-only mode on 25th Sep for 10 hours. Click here for more details

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

WICED™ Studio Forum Discussions

Browse the Community

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.

26582623 4100

Studio Bluetooth

Discussion forum regarding WICED Studio Bluetooth topics.

8124097 1554

Smart Bluetooth

Discussion forum regarding WICED Smart Bluetooth topics.

14989774 2746
filter icon

Featured Discussions

Sort by:
hoainguyen265
Wi-Fi Combo
I use module CYW54907 with  WICED Version: Wiced_006.006.000.0009   I alway got the socket disconnect event when download about 1.7Mb firmware file fr... Show More
StN__1917156
Studio Bluetooth
Keep getting those errors when connecting bonded Cysmart to CYW20719:Status : Connection Terminated Due to MIC Failure (0x3d)Encryption Status Event: ... Show More
iamwifi
Wi-Fi Combo
Following this discussion (link: https://community.infineon.com/t5/Wi-Fi-Combo/Looking-for-details-regarding-CYW43455-concurrent-Station-and-AP-operation/td-p/122651... Show More
maxm
Wi-Fi Combo
We are using the CYW954907AEVAL1F  board and it is stated that it has a TSF module that can adopt the timestamps from the AP However when requesting t... Show More
avra
Wi-Fi Combo
Hi, I'm getting the following error while trying to compile for PSoC-6 Kit using WICED Studio 6.6 on Linux.   Unknown component: CY8CKIT_062. Stop.  ... Show More
jdreitzler
Wi-Fi Combo
We are using a STM32F4 MCU.  When UART2 RX receives a string of data, the SPI1 data ready interrupt activates. It is possible to use SPI and UART2 tog... Show More
LixinD_46
Studio Bluetooth
HiWICED platform: 6.0.0.43Chip Platform: CYW20719-B1Issue Description:When invoke the wiced_bt_dev_get_bonded_devices() API, the always return 0x1FA7 ... Show More
Chih-YuanC_26
Wi-Fi Combo
Infineon AIROC Wi-Fi/Bluetooth Combo STM32 Expansion Pack is an extension of the CMSIS-Pack standard established by Arm. The pack is compliant with th... Show More
zsilet
Wi-Fi Combo
Dear Infineon team, I am trying to capture the raw data from four I2S microphones running with the CYW943907AEVAL1F (not planning to use a codec). I a... Show More
mineronarrow
Wi-Fi Combo
Hi Customer is developing with Murata 1GC on WICED.  They are sending with ux_device_class_cdc_acm_write. It is blocking.  It will stuck if other side... Show More
Category Information

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.