Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB Forum Discussions

Browse the Community

filter icon

Featured Discussions

Sort by:
Translation_Bot
USB superspeed peripherals
System: win11 The driver has been properly installed, and the factory default routine can run normally when I2C is started or USB is started. Select U... Show More
jpm-janz
USB EZ-PD™ Type-C
Hello Infineon community. Im currently working on a project with a TUSB1046 instead of a PS8740. Changing the device adress and some registers worked ... Show More
Ivan_Lee
USB low-full-high speed peripherals
Hi, All,   as we known the FX2 and FX3 SDK contain Driver and C#/C++ lib for windows  platform.   Does Cypress Driver support windows 11 ?    Does Cyp... Show More
jnagy
USB superspeed peripherals
I am implementing a UVC application using a manual, 2 socket, many-to-one DMA. We are encountering output buffer overruns so I would like to send erro... Show More
jali
USB superspeed peripherals
Hello, I'm debug the CYUSB3014 evb board base on the an75779 demo code, when I enable the USB_DEBUG_INTERFACE in uvc.h, and install the driver, but wh... Show More
beewoo
USB EZ-PD™ Type-C
Hi,  I am using the CYPD3120 in a custom USB-C receptacle to DP sink design (4x DP1.4 lanes). This board will have an external MCU onboard, and given ... Show More
Moon_shi
USB superspeed peripherals
We want to test the Synchronous transfer mode, can you provide the example?The example in SDK is bulk mode,Is there a tutorial if we modify it, or jus... Show More
JStrihavka
USB low-full-high speed peripherals
Hello, I´m searchnig for solution how to convert MIPI C-PHY 1.0 camera signal (sony imx 586 trial lanes) to HDMI, have Infineon some solution like CYU... Show More
Koki
USB hosts hubs transceivers
Hello Support,   My customer want to use HX2LP. Can you tell me the recommended pattern for HX2LP? Best regards, Koki Show More
Translation_Bot
USB superspeed peripherals
CYUSB3014 is used, and its firmware is expected to be downloaded to the EEPROM through IIC, but the download failed. The EEPROM is 24LC1025-I/SN. The ... Show More
Category Information

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.