USB Forum Discussions
Browse the Community
USB low-full-high speed peripherals
Discussion forum regarding USB low-full-high speed peripherals topics.
USB hosts hubs transceivers
Discussion forum regarding USB hosts hubs and transceivers topics.
USB superspeed peripherals
Discussion forum regarding USB superspeed peripherals topics.
Featured Discussions
Hello
How can I download the FPGA Configuration Utility tool(see the attachment) for CYUSB3014?.I want to Configure the xilinx FPGA over CYUSB3014.
Thanks.
Show LessHi Infineon Community,
I am reviewing the second SPI pinout interface, and I've noticed some discrepancies between various figures and tables regarding the pinout of SPI port 1.
Below, I have included a comparison table and images from Document Number 002-31604 Rev. **, as found on the CY7C65214D-32LTXI webpage.
I believe the correct pinout is shown in Figure 4, as it represents the actual pinout of the package. Furthermore, Figures 5, 6, and 7 are consistent with Figure 4.
Please confirm if my understanding is correct and make any necessary corrections to the document.
Regards,
Luis Flores
Show Less
Hello,
Can the EZ-USB SX3 CYUSB3017-BZXI co-exist with PolarFire Microchip FPGA in the same electrical design although the SX3 Configuration Utility does not support the given FPGA?
Show Less
The Win10 CY4500 Analyzer 4.0.0 installer doesn't appear to include a driver for the hardware. Neither does the Firmware update utility or the support section on the CY4500 product page. There's clearly no driver or driver installer utility.
Other Infineon customers have reported this same problem for v4.0.0 and for earlier versions. There are responses over the years from tech support claiming that 4.0.0 and 3.1 include a driver. However, customers have clearly proven that no such driver has been included. Also, support has said over the years that they'll release a driver shortly but unfortunately that never happened. If a driver indeed exists we'd like to see evidence of this.
Could someone please provide the filename and a link where it can be downloaded? And an explanation for the community as to why Infineon as chosen not to include include drivers or a driver installer utility with their software, including the latest 4.0.0 software. And why the CY4500 user manual and Quick Start guide are contain wrong and misleading info in this regard.
This is a poor first impression for a customer. The level of apathy seems worse than at TI. Thanks.
Before, we used 16-bit Data Bus + UART + SPI + I2S data mode, so we connected UART_TX and UART_RX respectively to E5 and E4 pins.
Now we need to use 32-bit Data Bus mode, and we changed to connect UART_TX and UART_RX respectively to C2 and D5, while we edited the code to switch to 32-bit Data Bus mode.
We could receive signals from the UART (we sent instructions and could get responses), but we could not get a complete image.
We wonder if we miss some operations that we need to do.
Show LessHi there.
Our customer developed a base board based on our core CPU module, which uses USB4.0 bus to extend CYPD5225-96BZXI + JHL8040R to realize the TBT4 type-C functional interface.
But now the problem is: as long as the power on, TBT4 type-c connected to the USB peripheral, the motherboard will not start, and unplug the USB peripheral, the motherboard can start normally;
So to find out.
1.CYPD5225-96BZXI What considerations are needed for design;
2、CYPD5225-96BZXI Is there a relevant reference schematic?
3、D2 "I2C_SDA_SCB2 "、E2 "I2C_SCL_SCB2 " What is the address bit corresponding to this group of I2c signals? And our CPU module (as Master), I2C bus need to communicate with CCG5, what are the requirements of I2C address?
4、Our related schematic diagram
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/USB-EZ-PD-Type-C/CYPD5225-96BZXI-%E5%BA%94%E7%94%A8%E9%97%AE%E9%A2%98%E5%8F%8D%E9%A6%88/td-p/703112
Show LessOpen the EZUSBSUITE PC tool.
Could you please tell me, 1.suite installation and programming demo refer to that document .
2. GPIF II Designer installation and programming demos refer to that document.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%B6%85%E9%AB%98%E9%80%9FUSB%E5%A4%96%E8%AE%BE/FX3-1-3-3%E6%94%B9%E6%88%901-3-4/td-p/719450
Show LessHi,
We want to do a MIPI to USB 3.0 bridge for a IMX179 sensor.
We are interested only in images that are different from previosu one. So it would be very good to filter out (not send through USB 3.0 channel) those images that are "equal" (with some degree of flexibility) to the previos image. This way we use less the USB 3.0 pipe and save also host application capacity.
Is possible to make this with CX3?
Can we store the image in CX3 and then compare with the new one and compute some difference rank and decide whether to send or not the frame?
Thanks for your help
Show Less
Hi,
We are looking for a MIPI to USB 3.0 bridge to stream MJPEG video from an IMX179 sensor.
We need to support 3280x2464 @5FPS.
Can we use CX3 CYUSB3065 for that?
Show Less