Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB Forum Discussions

Browse the Community

filter icon

Featured Discussions

Sort by:
jeidi98
USB superspeed peripherals
Hello,   I tested the video output on the custom board with the firmware provided by the kba below. In order to exclude and test the image sensor, we ... Show More
UM
USB superspeed peripherals
I am using the FX3 KIT to implement a camera interface using the code found in AN75779. Can someone explain what it means to be told that a "DMA Reset... Show More
yano_4433086
USB superspeed peripherals
The BT601 format data of the f 5640 module has been successfully debugged according to the 《Infineon-AN75779 _How_to_Implement_an_Image_Sensor_Interfa... Show More
role_1685151
USB EZ-PD™ Type-C
Hello. I'd like to know detail HPI register about BCR-Plus. Below is HPI register in BCR HPI Utility user guide.  I don't find detail document. Let m... Show More
jali
USB superspeed peripherals
Hello, If the LV(HSYNC) is not continuous, is it ok? I attach the image   Show More
DaEr_349131
USB hosts hubs transceivers
Hi, the datasheet reads: > After TetraHub is configured in a high speed system, it is in single TT mode. The host may then set the hub into multipl... Show More
FuBe_4381791
USB low-full-high speed peripherals
Hello Infineon! I've implemented a FIDO CTAP 2.1 interface on an FX3s but I am getting very strange behaviour with it... I've posted in the FIDO commu... Show More
wind13
USB superspeed peripherals
I am learning the 3014 chip. And when I use USB Control Center,  I found three burning methods. Could someone explain the difference between RAM mode ... Show More
yh486choi
USB superspeed peripherals
I am using the GPIF2 function of FX3 to receive large amounts of data from an FPGA, and then I am transmitting this data to a PC via USB using the Bul... Show More
abraxton
USB EZ-PD™ Type-C
Hi, I am not able to use the CY4500 PD software on MacOS. The software launches but in some sort of corrupted state that leaves it non-functional. It ... Show More
Category Information

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.