USB Forum Discussions
Browse the Community
USB low-full-high speed peripherals
Discussion forum regarding USB low-full-high speed peripherals topics.
USB hosts hubs transceivers
Discussion forum regarding USB hosts hubs and transceivers topics.
USB superspeed peripherals
Discussion forum regarding USB superspeed peripherals topics.
Featured Discussions
i read the doc "AN73609",about how to develop example on linux.
but,i can`t find bulkloopapp which is mentioned in the doc.
anyone know where can i find that?tell me please.
Or anyone just has one,send me please.
thanks a lot ^ ^ .
Show LessI use the function as follows- CyU3PGpifSocketConfigure(0, CY_FX_PRODUCER_PPORT_SOCKET, 3, CyFalse, 0);
I am able to transfer for a very short amount of time before Flag B remains Low = Buffer Full. Watching both Flags on the oscilloscope both flags go low when the buffer is full but only flag A goes back up to show that the buffer is Not Full. Why does the signal not go back up?
I also used this implementation- CyU3PGpifSocketConfigure(0, CY_FX_PRODUCER_PPORT_SOCKET, 0, CyFalse, 0);
When changing the watermark value from 3 to 0 I had no issues and flag B matched up with flag A other than being about half a clk cycle faster.
Thanks!
I have make a usb 3.0 board but when it's powered or reseted, sometimes the pc driver is not loaded. (abot 1 time per 10 trials.) why?
When i use the cypress dvk board, same result is appeared.
I am using the Netmate U-511 pci-e card for usb 3.0 I/F.
Thanks for your help.
Show LessWe've got a Windows 8 machine we're testing with. When we try to perform SuperSpeed IN transfers from EP0 of the FX3, if the transfer is larger than the 512-bytes (the only EP0 packet size supported for SuperSpeed), the transfer times out. We can see this on our USB analyzer and the call fails in Windows.
We are not seeing this issue with Windows 7. Has anyone seen this behavior?
Show LessFellow FX3 enthusiasts,
GPIF II Designer available at http://www.cypress.com/?rID=59628. Please use it and let us know your feedback.
Cheers,
Anand
Show LessI debugged the example of SlaveFifoSync and change the prodSchID of UToP DMA Channel to:
dmaCfg.prodSckId = CY_U3P_CPU_SOCKET_PROD;
dmaCfg.consSckId = CY_FX_CONSUMER_PPORT_SOCKET
The firmware ran through and PC can recognize FX3, but on the PC Host software side: USBDevice->DeviceCount() return 0 and USBDevice->Open(0) return false, SlaveFifoSync UToP producer socket has to be USB_SOCKET, other than that the exceptional error may occur??
Show LessCyU3PDmaChannelConfig_t dmaCfg;
dmaCfg.size = (usbSpeed == CY_U3P_SUPER_SPEED) ? (size * CY_FX_EP_BURST_LENGTH) : (size);
dmaCfg.count = CY_FX_BULKSRCSINK_DMA_BUF_COUNT;
dmaCfg.prodSckId = CY_FX_EP_PRODUCER_SOCKET;
dmaCfg.consSckId = CY_U3P_CPU_SOCKET_CONS;
dmaCfg.dmaMode = CY_U3P_DMA_MODE_BYTE;
dmaCfg.notification = CY_U3P_DMA_CB_PROD_EVENT;
dmaCfg.cb = CyFxBulkSrcSinkDmaCallback;
As you can see, I can manipulate the size (where the "size" identifier in the compact "if" statement is the packet size chosen according to the USB speed) and count fields to obtain different performances. Here on the forum I read that the size of DMA buffer can grow up to 64k, but any value I replace the right side of dmaCfg.size assignment with doesn't work (it lets me compile but fails programming the device by the control center). The default value of CY_FX_BULKSRCSINK_DMA_BUF_COUNT is 8, with which I obtain a transfer rate of about 10MBps. Raising it to 252 (but not any further, cause it doesn't work) changes the transfer rate to about 14MBps.
Using the CyFxBulkLpAuto example I could reach a transfer rate of 40MBps. Can you tell me why it goes so slow, even if the transfer is one-side only?
p.s. as software application I'm using the default visual studio cpp application provided.
Thanks,
mrain
Show Less