From the forum, I found that there are a lot of post disscuss the AN75779 sample. But when I search the sdk folder , there are no AN75779 sample code , and from "http://www.cypress.com/?rID=57990" (related files ) I also can not find the sample .
There are only two samples about uvc "usbvideoclass" and "usbbulkvideoclass" . And from AN75779 , there is a file named "uvc.c ", but there are no files named uvc.c. Ago I think that the AN75779 should be developed by developers, but from forum, it seems that Cypress offer the source code .
Is the sample free?? if free how can I get it? thanks!
Dear Bob,
Thank you for your reply, and I have looked it before. However, there are only pdf SPECs. and other related resources are no source code which descriped in the PDF Spec.
So , I think there is may have a source code project , and there are a lot of engineers ask questions about the AN75779 project.
Or that it is a mistake about my realize? that the project should be developped by developers themslves ??
Thank you!
Hi,
Download and extract teh files AN75779.zip found in http://www.cypress.com/?rID=62824. You can see uvc.c under "AN75779\001-75779_0C\USBVideoClass\uvc.c". Please see attached img.
Regards,
Gayathri