Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

       From the forum, I found that there are a lot of post disscuss the AN75779 sample. But  when I search the sdk  folder , there are no  AN75779 sample code , and from  "http://www.cypress.com/?rID=57990"  (related files ) I also can not find the sample .  

   

   There are only two samples about uvc "usbvideoclass" and "usbbulkvideoclass" . And from AN75779 , there is a file named "uvc.c ", but  there are no files named uvc.c.   Ago I think that the AN75779 should be developed by developers, but from forum, it seems that Cypress offer the source code . 

   

 

   

   Is the sample free??  if free how can I get it? thanks!

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked
        Have a look here:   
http://www.cypress.com/?rID=62824   
   
Bob   
0 Likes
Anonymous
Not applicable

 Dear Bob,

   

    Thank you for your reply, and I have looked it before. However, there are only pdf SPECs. and other related resources are no source code which descriped in the PDF Spec.

   

   So ,  I think there is may  have a source code project   ,  and there are a lot of engineers ask questions about the AN75779 project. 

   

  Or that it is a mistake about my realize? that the project should be developped by developers  themslves ??

   

 

   

  Thank you! 

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

 Hi,

   

 

   

Download and extract teh files AN75779.zip found in http://www.cypress.com/?rID=62824. You can see uvc.c under "AN75779\001-75779_0C\USBVideoClass\uvc.c". Please see attached img.

   

 

   

Regards,

   

Gayathri

0 Likes