Previously I develop firnware of FX2P. It has a conception of auto commit for an in endpoint. If the packet end signal does not asserted and data are continuously written into the in endpoint. The data would be auto commited. What is the meanning of commit. Does it mean the end of a packet. Does the similarity exists for FX3? I remmeber I should set the auto commit option for FX2L, but I have not seen the setting of auto commit for FX3.
Another question is: Does one packet have to exclusively occupy a buffer no matter how short the packet is?
Solved! Go to Solution.
Hello,
COMMIT - Transfer of buffer handle from one block to another (For example, from GPIF II to USB).
The concept of AUTO/MANUAL COMMIT exists in both FX2LP and FX3. In FX2LP< the EPxAUTOINLEN
Data can only be committed in terms of buffers and not as individual bytes. So, even if a buffer is filled with a short packet, the entire buffer is committed.
Best regards,
Srinath S