- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hi guys,
I am now working on a FX3 board, this board is connected to 2 sensors, it's meant to get image data from them in a synchronous way, then output data to host via UVC.
Since this is a UVC app, so I use AN75779 as a reference, and make some amend to the sample code for AN75779.
The sensor is aptina AR0130, can only output 12-bit raw data. Since raw format is unidentifiable for host video application like Amcap, so I need to convert it to YUY2 before transmitting to host. I study the doc&code for some time, it seems this conversion process can only be inserted into CyFxUvcApplnDmaCallback. After the conversion code is added, however, it looks like the entire application stops outputting any UART message, or the app just crashes. it seems heavy overhead is not allowed in CyFxUvcApplnDmaCallback.
I realize this FX3+AR0130 probably can't output YUYV to host directly, is it right?
Thanks!
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hi Hemanth,
Thanks for your reply.
The conversion from raw data to YUY2 will cause too much compuatation, this is why it can't be implemented on FX3, right?
Alternatively, I can use other sensors which can support YUY2 output instead of simply raw ouput, this will make the processing on host unnecessary.
Regards,
Michael