Anonymous
Not applicable
May 30, 2017
05:54 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 30, 2017
05:54 AM
Hi,
I am working as a software Engineer and I'm quite new to the CY7C6801a / 128 pin and keil uvision. I already have working firmware program and chip is on our own circuit. We haven't change the firmware since very very long time so I don't know how to connect the chip with keil uvision 3 and debug on the board.If it is able to debug with this chip, I would like to know how to do it.
On our circuit board , there is a 6 pin debug connector . Pin connections are as follow:
Pin 1 -> TX0, Pin2 -> RX0, Pin3 ->TX1, Pin4 ->RX1, Pin5 -> Gnd, Pin6->3.3V.
To be able to debug the program, how should i connect ?Do i need the Ulink2 adapter to connect ? How can I convert the 10 pin Jtag to 6 pin connection that I currently have on board?
Many Thanks
Su
0 Replies