- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am performing read and write operations on spi flash with the cypress given example code.
(C:\Program Files\Cypress\EZ-USB FX3 SDK\1.3\firmware\serialif_examples\cyfxusbspidmamode).
I have made settings as following in venodr device mode.
for spi write,
bytes to tranfer ( wLength 😞 4096
bmRequestType = outendpoint 0x40
bRequest = 0xC2
wValue = 0x0000
wIndex = 0x1000 (4096)
I am getting control out transfer completed in the control center along with sent test data
is it mean spi write is happening successfuly?
for spi read,
bytes to tranfer ( wLength 😞 4096
bmRequestType = inendpoint 0xc0
bRequest = 0xC3
wValue = 0x0000
wIndex = 0x1000 (4096)
I am getting control in transfer completed in the control center.
but 4096 bytes are zeros.
spi is not reading actual sent test data.
why this is happeing?
thank you.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The size of the Flash S25FL127SABMFI101 is 16MB and not 16KB. Please check.
Regards,
Hemanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Before performing WRITE to FLASH, it has to erased.
So, referring to cyfxusbspidmamode example, you need to send vendor command 0xC4 with wValue=1, Lower byte of wIndex = Sector Number.
When you are doing write, why are you giving wIndex as 0x1000? Is it because you need to write to 0x1000 page address. If yes, then okay. I wanted to let you know that the wIndex here is not related to number of bytes you transfer.
Regards,
Hemanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello hemanth,
thanks for the reply.
In C:\Program Files\Cypress\EZ-USB FX3 SDK\1.3\firmware\serialif_examples\cyfxusbspidmamode readme.txt file,They have given as below for spi write and read,
wIndex = SPI flash page address (Each page is assumed to be of 256 bytes and the byte address is
computed by multiplying wIndex by 256)
if wIndex is not = 0x1000 ,what will be the value for windex for spi write and read and also for spi flash erase.
please let me know.
thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
If you are reading/writing from/to the Page 0 of Flash then, you can put wIndex as Zero, If it is from Page 1 then wIndex = 1 and so on.
If you want to perform Erase, then wValue = 1 and wIndex should be the sector number that you want to erase.
Regards,
Hemanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
S25FL127SABMFI101 flash from cypress has 16kbytes.each page is containing 256bytes totally 63 pages from 0 to 63 pages.
for the last page 63,wIndex = 0x0040.
but for higher values for wIndex ,i am able to read and write to spi flash with control center.how ?
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The size of the Flash S25FL127SABMFI101 is 16MB and not 16KB. Please check.
Regards,
Hemanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
你好!
我有一个问题请教。
我设计了一个CYUSB3014的实验板,连接电脑后controlcenter可以显示BootLoader
,烧写代码到RAM中,显示烧写成功,但是并没有重枚举。也就是说电脑没有任何反应,包括识别USB设备,或者装驱动之类的。
另外我烧写到ROM(24LC1025)中,显示烧写成功,然后跳线选择ROM启动,也同样没反应,这是什么原因呢?
烧写的软件,包括烧写ROM的软件也按照技术手册用elf文件转换ok了,是经过其他电路验证没有问题的。
我不清楚问题出在什么地方,该如何解决。
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
To isolate the problem, please load the following standard program to RAM and see if it is re-enumerating:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\basic_examples\cyfxbulksrcsink
You have to load .img file to FX3 and not .elf
If it is not re-enumerating you might have to look into the schematics. You can refer to AN70707 and also FX3 Super speed explorer kit schematic as reference
Regards,
Hemanth