fx3 csi virtual channel

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
yoco_4642236
Level 1
Level 1
First reply posted First question asked Welcome!

Hi

 

can the FX3 get CSI virtual channel input

0 Likes
1 Solution

Hello,

CX3 does not support virtual channel feature of MIPI CSI-2 specification. Please refer to Question 6 of the following KBA which mentions this:

https://community.cypress.com/t5/Knowledge-Base-Articles/CX3-Hardware-Frequently-Asked-Questions-KBA...

Best Regards,
Jayakrishna

View solution in original post

0 Likes
3 Replies
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello,

I understand that you are referring to MIPI CSI 2 interface support on FX3. Is my understanding correct? If yes, FX3 supports GPIF II interface (parallel interface) for interfacing with sensors. It doesn't support MIPI CSI2 interface. Please refer to FX3's datasheet for more details https://www.cypress.com/file/140296/download 

You can use a FPGA between MIPI CSI 2 transmitter and FX3 for MIPI CSI2 to parallel interface conversion. You can also refer to this KBA for reference USB2.0 Camera Interface Using FX2LP™ and Lattice C... - Cypress Developer Community   Please note that this KBA is for FX2LP and is pointed just for reference.

Please let me know if any queries on this.

Regards,
Rashi
0 Likes

I was referring to CX3. sorry for the mistake.

Can the CX3 support virtual channel and if yes up to how many?

 

thanks

0 Likes

Hello,

CX3 does not support virtual channel feature of MIPI CSI-2 specification. Please refer to Question 6 of the following KBA which mentions this:

https://community.cypress.com/t5/Knowledge-Base-Articles/CX3-Hardware-Frequently-Asked-Questions-KBA...

Best Regards,
Jayakrishna
0 Likes