Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Yvan
Level 2
Level 2
First solution authored 10 sign-ins 5 replies posted

I'm trying to use two 8-bit cameras, connected to the FX3 to form a binocular camera, I have followed infineon-AN75779_how_TO_implement_AN_image_senSOR_interFACE_with_EZ-USB_FX3_IN_A_USB_VIDEO_class_ (UVC) _framework-ap PlicationNo document, but still no image.

0 Likes
1 Solution
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi,

I can see that there is video data coming from FX3 to the host.

Could you tell me if the individual sensor's resolution is 640*480, meaning total resolution from two sensor would be 2*640*480.

I see that there is a partial packet of 6436 in the bushound, is the same amount of partial packet seen always?

Could you also send us the descriptor file used in your application?

Best Regards,
AliAsgar

View solution in original post

0 Likes
8 Replies
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi,

Is one sensor working correctly with FX3?

Have you referred to section 9 of the application note you mentioned?

Could you confirm if both the sensors are transmitting data to FX3?

Best Regards,
AliAsgar

0 Likes
Yvan
Level 2
Level 2
First solution authored 10 sign-ins 5 replies posted

When one sensor works, it can work with FX3, I have made the descriptor changes according to section 9, two sensors have data to FX3, and through the Bus Hound software test, there is data transmitted to the host computer, however, after a while it will be Stuck, the VSYNC, HREF, PCLK signals of the two sensors are synchronized normally

0 Likes
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi,

Could you send different predefined patterns from each of the sensors, (For ex, 0xAA from sensor 1 and 0xBB from sensor 2) and then take the wireshark traces at the host PC to share the same with us.

Also please enable the debug prints and share the debug logs with us.

Which host application is used to view the data?

Best Regards,
AliAsgar

0 Likes
Yvan
Level 2
Level 2
First solution authored 10 sign-ins 5 replies posted

I use I2C for data transmission at the same time, and AMCAP for image acquisition

0 Likes
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi,

Could you answer the questions I have asked previously?

Best Regards,
AliAsgar

0 Likes
lock attach
Attachments are accessible only for community members.
Yvan
Level 2
Level 2
First solution authored 10 sign-ins 5 replies posted

HI,I'm so sorry i don't know why i can't enable uart for debugging and i can't send the pre-defined patterns from each sensor, but i can send you the data from the fx3, i'm using usb 3.1, for the data transmission, the resolution of the two sensors is 640*480

0 Likes
Yvan
Level 2
Level 2
First solution authored 10 sign-ins 5 replies posted

HI, I can continue to try to see if I can use uart for debugging

0 Likes
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi,

I can see that there is video data coming from FX3 to the host.

Could you tell me if the individual sensor's resolution is 640*480, meaning total resolution from two sensor would be 2*640*480.

I see that there is a partial packet of 6436 in the bushound, is the same amount of partial packet seen always?

Could you also send us the descriptor file used in your application?

Best Regards,
AliAsgar

0 Likes