Hi,
I want to generate a unique serial number for each my cx3 device,I have set according to the instructions on the following pages,but i can not get the serial num from device instance path,is there any place should i change?
Adding serial number descriptor to FX3 firmware
Re: CX3 UVC-CDC - Identifying the CDC COM port
i have change code as follow:
1. set serial num to 0x03 in descripter:
const uint8_t CyCx3USB30DeviceDscr[] =
{
0x12, /* Descriptor size */
CY_U3P_USB_DEVICE_DESCR, /* Device descriptor type */
0x00, 0x03, /* USB 3.0 */
0xEF, /* Device class */
0x02, /* Device Sub-class */
0x01, /* Device protocol */
0x09, /* Maxpacket size for EP0 : 2^9 */
0xB4, 0x04, /* Vendor ID */
0xC3, 0x00, /* Product ID */
0x00, 0x00, /* Device release number */
0x01, /* Manufacture string index */
0x02, /* Product string index */
0x03, /* Serial number string index */
0x01 /* Number of configurations */
};
2.define serial num in firmware:
const uint8_t CyFxUSBSerialNumDesc [] =
{
0x1A, /* Descriptor size */
CY_U3P_USB_STRING_DESCR, /* Device descriptor type */
'0',0,'0',0,'0',0,'0',0,'0',0,'0',0,
'0',0,'0',0,'0',0,'A',0,'A',0,'A',0,
0,0, /* long word align */
};
3. set descriptor in firmware
/* String descriptor 0 */
status = CyU3PUsbSetDesc(CY_U3P_USB_SET_STRING_DESCR, 0, (uint8_t *)CyCx3USBStringLangIDDscr);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rAppInit:Set_STRNG_Dscr0 Err = 0x%x", status);
CyCx3AppErrorHandler(status);
}
/* String descriptor 1 */
status = CyU3PUsbSetDesc(CY_U3P_USB_SET_STRING_DESCR, 1, (uint8_t *)CyCx3USBManufactureDscr);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rAppInit:Set_STRNG_Dscr1 Err = 0x%x", status);
CyCx3AppErrorHandler(status);
}
/* String descriptor 2 */
status = CyU3PUsbSetDesc(CY_U3P_USB_SET_STRING_DESCR, 2, (uint8_t *)CyCx3USBProductDscr);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rAppInit:Set_STRNG_Dscr2 Err = 0x%x", status);
CyCx3AppErrorHandler(status);
}
status = CyU3PUsbSetDesc(CY_U3P_USB_SET_STRING_DESCR, 3, (uint8_t *)CyFxUSBSerialNumDesc); //add this line
BR,
Solved! Go to Solution.
Hi,
I have tested using the following example:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\serialif_examples\cyfxusbuart
My Serial Number Descriptor is as follows:
Using the above, below is the result:
You can see that the serial number is updated.
Please try with this example first.
Regards,
Hemanth
Hi,
I have tested using the following example:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\serialif_examples\cyfxusbuart
My Serial Number Descriptor is as follows:
Using the above, below is the result:
You can see that the serial number is updated.
Please try with this example first.
Regards,
Hemanth