Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
FrSe_4506631
Level 1
Level 1
First like received

I followed the CyUSB Suite for Linux document on Ubuntu 14.04, installed Qt4 and libusb 1.0, built the cyusb library. Tried to program the FX3 with cyfxbulksrcsink, write data at end point 0x01 and it worked fine. But when try to read from 0x81, it suppose to return some constant data, but I always read back nothing.

This works on Windows. Do you anything special needs to be done for this to work?

Thanks,

Frank.

4 Replies
Hemanth
Moderator
Moderator
Moderator
First like given First question asked 750 replies posted

Hi Frank,

Did you write your own application to do the transfers? If yes, can you please share the code?

Regards,

Hemanth

Hemanth
0 Likes

Hi Hemanth,

I didn't write my own code, I just used the provided sample. Tried the cyfxbulklpautoenum and when I write to 0x01 end point, able to read what's been written from 0x81. But the cyfxbulksrcsink just does not work.

Please provide any advice to trouble shoot.

Thanks,

Frank.

0 Likes

Hello Frank,

Can you please share the USB Bulk Source Sink project that you built in Linux?

Did you use the same image file that built-in Linux to test in Windows Platform and it worked in Windows and not worked in Linux?

Regards,

Sridhar

0 Likes

Hello Frank,

Is the issue solved?

Regards,

Sridhar

0 Likes