Recent discussions
Hi,
I am able to stream 4160x3120 @20fps over USB 2.0 with my cx3 based custom board. My goal is to capture the still but while I am trying to capture still, the app is getting stopped instead of capturing. Sometimes it is capturing image but it is totally black(it is giving unsupported format error in photos app).
I have observed UART logs which shows Commit buffer failure. Log is as follows -- AppStop AppStart AppStop... Commit buffer failure.
I have referred related threads but I couldn't solve it.
Please find What I did...
1. I am following method 2 of UVC to capture the still. I have configured it in my configuration descriptor( Class-specific Video Streaming Input Header Descriptor).
2. DMA size that I am using is 256KB (without 2-stage bootloader)
3. DMA buffer size that I am using is 48KB and buffer count is 3.
By 2 and 3 steps I would have over come the Commit buffer error but I couldn't.
I would like to know
1. Do I need to mention still capture method in each and every resolution descriptor? Though i have mentioned there also but no use.
2. I heard that increasing H-blanking will solve Commit buffer error, Can I have an alternative for this(because sensor settings are not accessible for some reasons)
3. Why the app is getting stopped while trying to capture image, does fps creating any bad influence?
Help is most appreciated.
Thank you,
Abdul.
Show LessHi
I'm currently having trouble trying to debug on a EZ-USB FX3 SDK. I have followed the instructions in the user guide but nothing seems to make it work properly. I am using a Olimex ARM_USB_TINY_H on the ARM and OlimexODS version of OpenOCD 0.6.1 with the Cypress EZ USB Suite version of Eclipse. (This is the only verison of OpenOCD that seems to work)
I am using the configuration file for the debugger from the OlimexODS package which was downloaded from their website, along with the arm926ejs_fx3.cfg in the files provided with the FX3 SDK which I modified to work with ftdi interface. I will attach them.
When I connect, I get a lot of warnings and errors in the console - also see attached file.
When the Eclipse debugger loads, I am stuck in the CyU3PFirmwareEntry. I have no options to step, and when I run it does nothing except stay at CyU3PFirmwareEntry. I believe it's supposed to run to main and break there but I am not seeing this. (Screenshot attached)
Any help is greatly appreciated and let me know if you need any more information that I might have missed.
Thanks.
Show LessHi!
We have for a customer designed a camera system based on the FX3 and the AN75779 sample code, with minor modifications.
Our customer reports that sometimes the FX3 stops streaming and gets non-responsive.
Restarting the software on the PC sides does not help.
Rebooting the PC does not help.
The only thing that helps is powercycling of the FX3 (either by unplugging and again plugging in the USB or by powercycling of the PC)
SInce this application is running remotely and not supervised, powercycling is not possible with the current design.
We have not yet been able to do any logging when this happens, but have in the meanwhile some questions.
Are there any know problems with the AN75779 implementation that could lead to this kind of sympthoms?
(We have implemented a watchdog in the FX3 that should restart the FX3 if asserted)
Is there some reset handling for the USB interface implemented in the An75779?
I think there are eset USB messaged sent to the FX3 - is that something that the FX3 will act on?
Regards,
Magnus Peterson
Show LessHello.
I am using FX3 - CYUSB3035. It works as the "cyfx3s_fatfs" example, but an error occurs.
* Using the example
* Block diagram of structure
* Schematic
* Error message
? : CY_U3P_ERROR_INVALID_UNIT, /**< Non-existent storage partition selected for transfer. */
I think it's the error message.
Other than the "ls" command, it doesn't work.
Please check if there is any problem with F/W & H/W
Show Less
Infineon's EZ-USB FX3S and SD3 support both support RAID 0 and RAID 1. Do any products support other RAID levels, specifically RAID 5?
RAID 0 is Block-level striping without parity or mirroring
RAID 1 is Mirroring without parity or striping
RAID 5 is Block-level striping with distributed parity
Greg
Show LessHello,
I am using GPIO pins to generate some on off sequence on pin. But while generating it sometimes my sequence gets stretched as attached in file. here i am using Simple GPIO.
I am using for loop for the same.
for(i=0; i<=7; i++)
{
CyU3PGpioSimpleSetValue(45,CyTrue);
CyU3PBusyWait (1);
CyU3PGpioSimpleSetValue(45,CyFalse);
CyU3PBusyWait (1);
}
Let me know what i am missing.
Show LessHi team,
I added different resolutions to my custom camera board with the help of this link .
I have taken care of probe control settings and descriptor settings while adding different resolutions.
Currently I am facing some issues and I would like to have a help from you.
1. I can able to stream 13MP resolution over USB 2.0 but for some lower resolutions like VGA I'm getting black screen in AMCap. But I am getting image in windows camera app, why is this happen ? Did I miss anything?
2. 13MP resolution streaming is perfectly being done and I have added still capture capability to it. When I try to capture image, the streaming is getting interrupted and on to UART log side I'm getting DMA_RESET(continuously starting and stopping the App). May I know why this happening?
Your help is most appreciated.
Thank you,
Abdul.
Show Less
I need to use the cyusb3kit-003 SuperSpeed Explorer kit to develop a "logic analyzer" that writes from 16 bit parallel input to windows disk through USB3. I have a USB2 device that takes data to a buffer, but the readout won't keep up with input.
It is simple. I need an EXE file for execution under windows command prompt that takes data and writes to binary disk like my current unit. I am not a programmer, so I need to find someone to do the programming. I use a high level language to read the binary file and process it.
The web pages lead me in endless circles, and the associates list does not seem to know about the SuperSpeed device. Short of learning binary coding which I do not have enough time to do, I see no help.
Show Less
I've been trying to implement a SPI interface on FX3 in order to reprogram a flash IC driving an FPGA, similar to the implementation described in AN84868 . I've been able to read from and write to the flash chip when I load slightly modified* versions of the USBFlashProg and UsbSpiDmaMode examples into RAM, but if I build the same code as an I2C image and load it onto the FX3's I2C boot EEPROM, the FX3 crashes and returns nothing but code 997 as soon as I make a SPI request.
Things I've already tried:
1) All three available speeds, 64k and 128k I2C sizes in elf2img.exe's -i2cconf argument. Of the settings that could be successfully programmed to the I2C EEPROM, none of them had any discernible effect
2) Performing a SPI read operation while the SPI mux select pin* is pulled low; this doesn't cause a crash, but the data returned is all zeroes (for obvious reasons)
3) Changing the DMA timeout value from 0xFFFFFFFF to 0x00004000 -- no effect at all
4) Checking SPI busy status before performing a SPI read operation -- the check busy status command also crashed the FX3.
5) Using I2C in register mode instead of using DMA -- no effect
6) Commenting out all of the "if (status != CY_U3P_SUCCESS) {return status;}" statements -- no effect
7) disabling and reinitializing SPI and I2C before making any SPI requests -- no errors were returned during DeInit and Init calls for I2C and SPI, but the crash happened as soon as I made a SPI request
8 ) Commenting all I2C functions out and setting io_cfg.useI2C to CyFalse.
I'm out of ideas. I can't think of any reason that booting from I2C should have any impact on SPI operation in a way that wouldn't be solved by one of the things I tried. Has anyone else encountered anything like this?
* An external mux select needs to be pulled high to give the FX3 access to the SPI flash IC, but it's driven from a GPIO so I just use CyU3PSetSimpleConfig() with .outValue set to CyTrue.
EDIT: I was able to capture oscilloscope readings on the MOSI trace between the FX3 and the SPI flash. Here's a capture of a CY_FX_RQT_SPI_FLASH_ERASE_POLL when the image is loaded via RAM:
and here's the same command running the exact same image booting from I2C:
I've seen this happen on every command -- if the FX3 was booted from I2C, the MOSI line has a lower-voltage "echo" after each pulse. Additionally, there is no activity at all on the MISO line after booting from I2C no matter what commands are sent.
When a SPI read request is made after booting from I2C, the FX3 continually broadcasts the same pulse and echo until power is removed, suggesting that the crash is happening because the FX3 is stuck in a loop attempting to make contact with the SPI flash IC. However, setting a timeout in the SPI configuration settings does not fix this issue.
Show LessI have an FX3S design which I would like to transition from I2C boot to eMMC boot (connected to the Sib port). I see information in the manual on how to attempt that directly with the PMODE pins. Unfortunately, my design uses a version of the two-stage bootloader (I2C) to allow device updates and the boot_fw library doesn't support Sib boot, is that true?
Is it possible to implement a two-stage bootloader with only the eMMC? I would like to eliminate my I2C eeprom components.
Thanks!
Show Less