Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Sort by:
Translation_Bot
USB superspeed peripherals
System: win11 The driver has been properly installed, and the factory default routine can run normally when I2C is started or USB is started. Select U... Show More
jnagy
USB superspeed peripherals
I am implementing a UVC application using a manual, 2 socket, many-to-one DMA. We are encountering output buffer overruns so I would like to send erro... Show More
jali
USB superspeed peripherals
Hello, I'm debug the CYUSB3014 evb board base on the an75779 demo code, when I enable the USB_DEBUG_INTERFACE in uvc.h, and install the driver, but wh... Show More
Moon_shi
USB superspeed peripherals
We want to test the Synchronous transfer mode, can you provide the example?The example in SDK is bulk mode,Is there a tutorial if we modify it, or jus... Show More
Translation_Bot
USB superspeed peripherals
CYUSB3014 is used, and its firmware is expected to be downloaded to the EEPROM through IIC, but the download failed. The EEPROM is 24LC1025-I/SN. The ... Show More
haines
USB superspeed peripherals
Dear ifx teams: 1、usb的并口控制信号,就是USB_PHY_CTL【0-12】组内等长,误差±5mil;usb的并口数据,就是USB_PHY_DQ【0-31】组内等长,误差±5mil,这个等长合理吗? 2、USB_PHY_CLK和数据线等长还是和控制线等长? 3.并口的阻抗需要控... Show More
Stalker
USB superspeed peripherals
Hello, I am starting work with FX3 chipset, and follow appnote AP75705 example USB Bulk Loop Auto. I have compile the code; Program the board  via "Co... Show More
fventuri
USB superspeed peripherals
I am working on a project where we would like to connect an ADC directly to the FX3 and send to the host only alternate samples (i.e. every other samp... Show More
jali
USB superspeed peripherals
Hello, I'm debuging the USB MSC on the CYUSB3014 board, I check the demo code(USBMassStorageDemo), it define the buffer on the ram, I want to write al... Show More
weiminwang
USB superspeed peripherals
Usually, actions in the active state will be performed in every clock cycle, and the transition conditions are checked on each clock edge. My question... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.