USB superspeed peripherals Forum Discussions
Does anyone know if it is OK to leave the USB 3.0 1.2V supply pins (and associated logic powered by those pins) unconnected if the FX3 is to be used only for USB 1.1/2.0 communication? I didn't see anything in the datasheet or schematic design checklist (AN70707).
Thanks,
Steve
Hello! I'm working on a USB-to-GPIF interface and I've noticed a problem. When I have DR_ADDR, DR_DATA, and DR_GPIO actions together in the same state, the data and GPIO lines update immediately as expected but the address lines update one clock-cycle later (with synchronous GPIF). I am using the address counter as the source. Is there a way to fix this to have the address lines drive at the specified time?
Thanks,
Brett
Show LessHi,
Can I improve the download speed via interrupt endpoint (I am using it to configure FPGA), the same way that is explained in
http://www.cypress.com/?app=forum&id=167&rID=59529 or http://72.3.161.91/?app=forum&rID=63024 ?
I have four endpoints in total. Two bulk (slave FIFO GPIF) and two interrupt, I would like to improve the download speed of the OUT interrupt edn point, but when I configure the cypress with the img file, windows cannot recognize the device anymore.
Thanks,
Nazila
Show LessHi,
Can I improve the download speed via interrupt endpoint (I am using it to configure FPGA), the same way that is explained in
http://www.cypress.com/?app=forum&id=167&rID=59529 or http://72.3.161.91/?app=forum&rID=63024 ?
I have four endpoints in total. Two bulk (slave FIFO GPIF) and two interrupt, I would like to improve the download speed of the OUT interrupt edn point, but when I configure the cypress with the img file, windows cannot recognize the device anymore.
Thanks,
Nazila
Show LessHi,
I am using slave fifo GPIF II. I would like to be able to discard (delete) the content of the GPIF FIFOs from CYUSB3014. I am using the "CyU3PUsbFlushEp" for both the producer and consumer. But the FIFOs stay unempty! How can I do this?
Thanks,
Nazila
Show LessLooking at the supply bypass recommendations there are discrepancies hopefully someone can address. On the AN70707 HW Design Guidelines & Schematic checklist, Section - Device Supply Decoupling, U3TXVDDQ & U3XXVDDQ call for 22uF caps. However in the DVK schematics they are 2.2uF. Which is the correct recommendation? Thanks
Show LessFor the USB connections in the DVK board schematic, in page 9, the pins from FX3 side: SS_RX_P and SS_RX_N are connected to MICRO_SSRX- and MICRO_SSRX+ on the USB microB side respectively. Is this a typo? Or they have to be swapped for the connection?
Thanks.
Show LessHi,
we use SlaveFifoSync this example,How to clear the DmaChannel Buffer and Endpoint memory,
I use CyFxSlFifoApplnStop () andCyFxSlFifoApplnStart() to do, Spend a long time.
LIAN,Thanks.
Show Less