Hello experts,
I trying to design a host application to update the firmware of my device. I am following CyControlCenter.pdf provided in the SDK -->C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\c_sharp.
I have struck up at one place i.e., the devices which are in bootloader mode can only be detected by Control center and shown up in Device tree. I am trying to imitate this behavior in such a way that my application needs to detect the devices which are in device mode and needs to communicate with it further.
Is it possible to communicate with devices which are in device mode?
If yes, could you please give a hint to do this?
Thank you,
Shafi.
Show LessPlease clarify that 24-bit GPIF bus support is fully supported in FX3.
The FX3 datasheet mentions (in multiple places) that the FX3 supports a 24-bit GPIF bus. It says it on pg1 when summarizing the features as well as on pg9 where it describes the GPIF bus in greater detail.
In the revision tracking section of the datasheet (pg55), revision E says " Removed 24 bit data bus support for GPIFII"
Greg
Show LessWe've created a custom board containing a CYUSB3014-BZXC with a GPIF interface attached to a Spartan 7 FPGA. My GPIF state machine is very similar to the SlaveFifo design desribed in AN65974, with two primary differences:
1. I've removed the SLCS signal. We use a GPIO pin to tell the FPGA when the host application has enabled the interface. The FX3 still provides FLAGA and FLAGB and they are connected to Current_Thread_DMA_Ready and Current_Thread_DMA_Watermark. The FPGA controls the remaining signals (SLRD#, SLOE#, SLWR#, PKTEND#, and A[1:0]).
2. The FX3 sources PCLK but it is still a slave design. This was done so that a separate GPIF design can be used to configure the FPGA in Slave SelectMap mode.
When the host initiates a data transfer the FX3 firmware creates a multichannel DMA between USB OUT endpoint 3 and GPIF threads 2 and 3 and allocates two 16K buffers if the transfer involves OUT data. If the transfer involves IN data then the firmware creates a multichannel DMA between USB IN endpoint 4 and GPIF threads 0 and 1 and allocates two 16K buffers. If the transfer is bi-directional then both DMA channels are created and the buffer sizes are the same as in the unidirectional case.
When the host wants to transfer data it first sends a command to the FX3 to tell it to enable the GPIF interface. This will cause the PIB clocks to be configured and the state machine to be loaded, and then the enable signal to the FPGA is driven to a '1'.
The host test application can be configured to perform OUT only transfers, IN only transfers, or bidirectional transfers with data verification in a loop. Each time the host enters this loop it sends a 16 byte command to the FPGA that tells it which direction the transfer will be, and if data is to be written too/read from a 16K BRAM FIFO that exists inside the FPGA or data read from the FPGA Is simply discarded, and data written from the FPGA is from a counter instead of the FIFO. The command includes OUT and IN byte counts so that the FPGA knows how much data to transfer in each direction.
After the command is downloaded the bulk data transfer begins. For OUT only transfers the data is read by the FPGA over the Slave Fifo interface and discarded. For IN only transfers the FPGA will writes the value of an internal counter to the FX3. For bidirectional transfers the FPGA first reads a buffer of data from the FX3 (address 2 or 3, alternating on each FX3 read, always start on address 2) into the BRAM FIFO and then writes the BRAM FIFO to the FX3 (address 0 or 1, always starting on address 0, alternates on each FX3 write, always starting on address 0). The process is repeated with addresses toggling between each transfer until all data is transferred.
Once the bulk data transfer completes several smaller transfers are performed to read statistic registers that are inside the FPGA. Those statistics include how many times the FPGA thinks that it asserted SLOE, SLRD, SLWR, and PKTEND. They also include the last 32 OUT addresses, the last 32 IN addresses, and in the case that the transaction is aborted by the host due to timeout, it also includes the address that the FPGA thinks that it will read or write next and the count of words presently in the BRAM FIFO.
If the test is supposed to be performed for more than one iteration then it loops.
Testing has shown that unidirectional OUT transfers and unidirectional IN transfer work reliably at 100 MHz. Bidirectional transfers work reliably at 89.6 MHz, but will fail randomly when PCLK is set to 100 MHz (100.8).
When the bidirectional transfers fail the statistics collected from the FPGA show that the FPGA last received a buffer from the FX3 and wrote it into the BRAM FIFO and is in a state where it's waiting for FLAGA to indicate that there is an IN buffer available to write data to. The count of words in the BRAM FIFO is equal to 4096 and I can see that during the last 32 OUT's and IN's there have been now repeated READS or WRITES to the same address two times in a row, meaning that it correctly toggles the address each time. I can also see that the FPGA logic is waiting for an IN buffer on the correct address. However, it never receives one.
In the FX3 firmware I've setup a DMA callback on the producer endpoint (consumer was never signaled) of both the OUT and IN DMA channels. Each time the producer event occurs I increment the count of bytes transfered by 16K, but never exceeding the total size of the transfer, which may not be a multiple of 16K. The host application receives these counts after the transaction completes, or is aborted (fails). From this I can see that the FX3 thinks that it received one less 16K buffer than the FPGA thinks that it sent. This makes me think that the signal timing may be off and that a SLWR is being missed by the FX3. Is there a way for me to determine how many bytes are stored in the DMA buffer associated with socket 0 and socket 1 so that I can see if a word was missed?
Some other observations:
Our firmware outputs the USB PHY and Link error counts over UART once per second. During an OUT only transfer the error count stays at 0 when I run a large number of transfers. This is also true for an IN only transfer. However, when I perform the bidirectional transfer I see PHY errors reported each second. Why are there PHY errors during bi-directional transfers but not the uni-directional transfers?
1000 ms PHY errors = 12
1000 ms LINK errors = 0
1000 ms PHY errors = 6
1000 ms LINK errors = 0
1000 ms PHY errors = 11
1000 ms LINK errors = 0
1000 ms PHY errors = 12
1000 ms LINK errors = 0
1000 ms PHY errors = 6
1000 ms LINK errors = 0
1000 ms PHY errors = 12
1000 ms LINK errors = 0
1000 ms PHY errors = 12
1000 ms LINK errors = 0
1000 ms PHY errors = 6
1000 ms LINK errors = 0
1000 ms PHY errors = 10
1000 ms LINK errors = 0
1000 ms PHY errors = 11
1000 ms LINK errors = 0
1000 ms PHY errors = 12
I've registered a callback function to see if CYU3P_USBEP_SS_RESET_EVT occurs, but it does not.
Larger (160MB) bidirectional transfers fail much more frequently than small (16MB).
Our firmware sets the OUT and IN endpoint burst size to 16 by default. If I change it to 1 (disable burst) on both of the endpoints then bidirectional transfers NEVER fail, even at 100 MHz. I still see the same number of PHY errors that I did at 100 MHz so I'm not sure that the PHY error count is what ultimately causes IN transfers to stop.
Are the PHY errors what ultimately causes the IN transfers to stop, or is it something else?
Any suggestions on how to further debug this problem? I tried to capture the bus traffic with the Ellisys EX350 but that's very difficult because it seems to prevent the data transfer from failing, or at least makes it fail much less often, and the amount of data is so large that the capture stops.
Thanks,
Michael
Hi,
I've created a custom bootloader for the CYUSB3014-BZXC using the Cypress Boot API. The bootloader supports application firmware download to RAM using a vendor request very similar to the Fx3BootAppGcc example. The host downloads the application firmware to the device in 4096 byte chunks. Testing has shown that application firmware download works reliably across many different hardware configurations and operating systems. However, I have identified a system and OS where firmware download fails unless I reduce the chunk size to 512 bytes.
I have a system that runs both Ubuntu 20.04.4 LTS 64-bit and Windows 10 64-bit. Firmware download works correctly under Windows 10, regardless of connection speed. However, it fails under Ubuntu when the device is connected through a USB 3 cable to a USB 3 port. I performed a packet capture with the Ellisys EX350 and found that the bootloader acks the first 512 bytes of a 4096 byte setup request but then fails to acknowledge the next 512 bytes of the data stage after previously sending an ERDY for control endpoint 0.
I added some UART debug prints and found that the firmware is getting stuck inside of CyFx3BootUsbDmaXferData and will eventually return CY_FX3_BOOT_ERROR_ABORTED, but only after the next setup packet is received, which doesn't happen until our software is restarted because it errors out when the host is unable to complete the previous control transfer.
If I connect the board to the same USB port using a USB 2.0 cable then firmware download is successful.
If I connect the board to the same USB port using a USB 3.0 cable and run the software in Windows 10 instead of Linux, then the firmware download is successful.
If I modify our host software to send data in 512 byte chunks then firmware download succeeds but it takes approximately 2.2 seconds to complete instead of 286 milliseconds. Therefore, reducing the transfer size is not an acceptable solution.
I performed packet captures in both Windows and Linux but couldn't identify any notable differences in the first control transfer, other than it succeeds in Windows and the device fails to respond to the OUT packets in Linux.
Can someone please help me figure out why this is failing in Linux? Obviously the host controller driver is different, but like I said I can't see any obvious differences in bus activity.
I can send the bus activity log but the files are too large to attach so they will need to be sent via OneDrive, which requires an email address.
Thanks,
Michael
Hi,
I've written a custom bootloader for the CYUSB3014-BZXC using the Cypress Boot API. We've been using this bootloader without issue for the past couple of months. However, someone recently plugged the board into a USB 3.1 host controller using a USB 2.0 cable. Upon doing so we discovered that in USB 2.0 mode the device stops responding to standard requests after being suspended and then resumed. The traffic on the USB bus was captured with an Ellisys EX350 and shows the following transactions:
1. get device descriptor (success)
2. set address (success)
3. get device descriptor (success)
4. get configuration descriptor (success)
5. get BOS ddescriptor (success)
6. get serial number descriptor (success)
7. get language ID descriptor (success)
8. get product descriptor (success)
9. set configuration 1 (success)
10. LPM transaction (success)
11. Suspended
12. Resume
13. get language ID descriptor x 6 (failure)
14. get manufacturer descriptor x 6 (failure)
15. get product descriptor x 6 (failure)
UART Debug message prints from the firmware show the following:
Initializing FX3 Boot Firmware 1.6
Boot FW Event: CY_FX3_BOOT_USB_IN_SS_DISCONNECT
Boot FW Event: CY_FX3_BOOT_USB_SUSPEND
Boot FW Event: CY_FX3_BOOT_USB_RESET
Boot FW Event: CY_FX3_BOOT_USB_RESET
Boot FW Event: CY_FX3_BOOT_USB_RESUME
Are there any special actions that the firmware must take when it receives CY_FX3_BOOT_USB_SUSPEND or CY_FX3_BOOT_USB_RESUME in order to get the FX3 to ACK the control requests that take place after the the suspend and resume operations?
We also seem to experience the same problem when running the application firmware (uses Cypress full API) when the device is plugged in with a USB 2.0 cable. The bus activity is similar:
1. get device descriptor (success)
2. set address (success)
3. get device descriptor (success)
4. get configuration descriptor (success)
5. get BOS ddescriptor (success)
6. get serial number descriptor (success)
7. get language ID descriptor (success)
8. get product descriptor (success)
9. LPM transaction (success)
10. Suspended
11. Resume
12. set configuration 1 x 3 (failure)
13. Suspended
So the same question applies for the application firmware: what steps must we take in firmware in order for control transfers to succeed after the device has been suspended and then resumed?
Some other information that you may find useful:
Operating system: Windows 10
Host Controller: Asmedia ASM3142
Hub: none
I appreciate any help you can provide.
Thanks,
Michael
Hello,
Our CX3 I2C is not working properly, looks like only sometimes in random we mange to communicate with our camera module. lookin at the signals we see that the rise time is high as well as the frequency is not as it should, it is 250KHz instead of 400KHz. this is with 10K pull-up resistors as it is in the reference design.
we tried changing the pull-up to 5KHz, this had an impact, mainly on the frequency which changed to 280KHz.
Then we saw in the FX3 checklist that it is recommended to use 2K pull-up (it is for flash but we decided to try) and the signal changed to 400KHz but the rise time is still bad
any suggestions? there is nothing on the I2C lines that is loading them (the signals remain similar with and without the camera module).
attached also the schematics and layout.
thanks,
Show Less
Hi,
I am working on a Denebola CX3 Kit which comes with a OV5640 image sensor. I used the sample application "Cx3UvcOV5640" and flashed the board. I am able to see the video on e-CamView and it works fine. I am trying to get some logs from the device so that I can view it on my serial console (Tera term). The USB COM port comes up on the PC, but I am not able to see any messages.
I am sending messages via the serial console using CyU3PDebugPrint(). CX3_DEBUG_ENABLED is also set to 1.
Any idea why I am not seeing the debug logs on my PC.
Please provide any examples to view serial logs.
Thanks and Regards,
Subbu
Show LessHi,
I am working on a Denebola CX3 Kit which comes with a OV5640 image sensor. I used the sample application "Cx3UvcOV5640" and flashed the board. I am able to see the video on e-CamView and it works fine.
I would like to control a peripheral, other than the camera I2C, which is connected to CAM_I2C_SDA and CAM_I2C_SCL on the MIPI connector.
How do I configure it and transmit/receive to the peripheral ?
I see the API CyU3PMipicsiInitializeI2c() which should initialize the I2C interface. How do I transmit and receive to this I2C interface. Is there any MipiI2c transmit and receive APIs available? Any examples you can point to me will be really helpful.
Thanks and Regards,
Subbu
Show LessHi,
I am currently working with CX3 device in order to get full-frame from CIS sensor. I have enabled several Processing Units(PU) in order to have a handshaking with sensor, and control it.
It works fine in Windows, working under UVC. But I am having problems in Ubuntu, working under V4L2.
It is a few strange, because the device is running with the same firmware, so I guess there is something wrong either uvcdscr.c or uvc.c file.
Please, could you tell me if it's common having problems between UVC and V4L2? Have I to configure the Processing Units on different way?
I have attached both uvcdscr.c and uvc.c files.
Thanks so much.
Show LessHi,
I am using CX3 based custom board, I have written my firmware image in SPI flash and my board is enumerating as a device in SPI boot mode. But image streaming is not being done(getting black screen).
My DMA and timer getting restarted continuously. I followed this KBA and changed the timer period and I increased the DMA buffer size. Still I am unable to get image in AMCap or Camera app.
Please find the below log for your reference.
Can you help me in this regard?
Thank you,
Shafi.
Show Less