USB superspeed peripherals Forum Discussions
Hi,
I was wondering if there's any chance that in the future we can get the latest update of the EZ-USB FX3 SDK directly from a git repository instead of a zip file.
I would be nice to have an official github account with this SDK
Regards
Show LessI am using cyapi.lib in a C++ project in Visual Studio 2015. Everything builds, and seems to work OK, but I always get the following link warning when I build:
warning LNK4098: defaultlib 'LIBCMT' conflicts with use of other libs
I have looked online for solutions, but none of them seem to apply to my situation.
Does anyone know what might be causing this warning?
Is it something I can fix, or should I just suppress and ignore it (since my code seems to be working OK)?
Show LessIs there example code available that shows how to install Window's OS descriptors in the FX3 firmware, so that it automatically makes Windows use its WinUSB driver?
I'm trying to add the required string descriptor to the mandated index 0xEE, but I'm getting an 'index' error. How do I add that string descriptor to index 0xEE? (Do I need to create up to 0xEE dummy string descriptors? Actually, that is doubtful, The FX3 seems to allow 16 as its highest indes: due to: #define CY_U3P_MAX_STRING_DESC_INDEX (16) )
Kind regards,
~ Paul
Show LessDear sir:
I want to know if CYUSB3065 can support 120fps 720p,whether there is a corresponding reference design(such as OV4682 sensor)?
If not, whether there are other other solutions?
thank you!
Show Lesswe are designed usb sd3 based custom board. we have ported example illustrates the use of the FX3S firmware APIs to implement mass storage class device that allows access to SD/MMC devices connected to SD3 given along with SDK.kindly suggest how to make password protection of partion created in emmc card
Show LessHello,
I have 2 question about developing printer application with FX3
1. Does FX3 support multiple class driver ? such as description below
Using 2 interface descriptor which is Printer class and vendor class, and each interface could transfer Bulk IN, Bulk OUT.
2. Could you share me any FX3's example driver for printer?
Thank you in advancce.
Regards.
Show LessHi all,
I have the following doubts regarding xfer data and buffers.
1. I am sending Xfer data from the pc and I have set buffer count to 6. If i send 1 xfer command,how many buffers do i get(will I get the 6 buffers or only 1 buffer).
2.What is the minimum time between xfer commands.
3. Maximum How many buffers can I use
4.What happens If i send xfer data command too fast and buffer is not available
Regards
Arun
Show LessHi,
I wanted to know which chip the CYUSB3KIT-003 board uses. all i managed to know by reading datasheets and application notes is that the chip is CYUSB301X, and it doesn't tell very much since some of the FX3 chips have 16 bit data bus width. you know, actually i want to use the board for transfering the ADC data that i read by an FPGA to PC , so i concerned about the actual throughput that i can get from the board.
Show LessHello
We are trying to send data from C# application to spartan 6 board through USB fx3 and spartan 6 will write the same data through USB fx3 to c# application.
We are able to send the data but unable to receive it back.
For fx3 firmware i have used application note AN65974 and firmware code available with it.
Also i wanted to know which function to use #define STREAM_IN_OUT or #define LOOPBACK_SHRT_ZLP present in the firmware.
Looking for support on the above mentioned issue.
Thanks
Show Less