Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals

Recent discussions

Sort by:
amulya_nr
USB superspeed peripherals
Hi I am using FX3 USB superspeed hardware. I am trying to do file transfer from Master to Slave using cyusb_linux application. I have downloaded the l... Show More
rainmen747
USB superspeed peripherals
Is it possible to change DMA configuration while running and restart DMA? Below is a source that runs in 2-socket GPIF mode and runs fine. and I want ... Show More
Panneerraja
USB superspeed peripherals
Hi All,  I am using a custom board where Fx3 USB controller is connected to Xilinx FPGA. I am trying to create an board level Vhdl/Verilog test bench ... Show More
ViKu_2048416
USB superspeed peripherals
Hi, For my initial evaluation of USB3 Vision, I am using the source code shared in the forum. Using that source code, I am able to enumerate the devic... Show More
Wellington
USB superspeed peripherals
Hello, I have study to this thread and other multiple FX3 transmission. Some simple question to clarified as below: https://community.infineon.com/t5/USB-superspeed-peripherals/Multi-FX3-Usb-deivce/m-p/345350... Show More
Flute
USB superspeed peripherals
我使用的开发板是CYUSB3KIT-003。开发板在StreamerExample模式下正常启动后,PC端通过EP0端口给开发板发送一个字节,开发板响应代码如下所示: if(itype == 64 && itarget == 2 && ireq_type==66 && irequest ==... Show More
ThAl_4704151
USB superspeed peripherals
Hello all,  Most of the data I'm trying to transmit seems to be going between the FX3 and the other chip just fine, but I'm periodically getting zero ... Show More
lu_xiongbin
USB superspeed peripherals
If I need to use multiple endpoints of fx3, should I use them in order? That means I should use ep1, then ep2, ep3, and so on. Can I not use ep2, inst... Show More
user_1484456
USB superspeed peripherals
I have implemented a U3V camera with FX3014, but the CMOS sensor has DVP parallel interface. In order to use MIPI or LVDS CIS with high resolution, I ... Show More
LeoChen
USB superspeed peripherals
Hi, I am working with a sensor at 1280x720@30fps YUV422_8 output, I want to use 24bit-bus to transfer data. But when I set up this project, I found th... Show More