Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Sort by:
Translation_Bot
USB superspeed peripherals
CYUSB3014 is used, and its firmware is expected to be downloaded to the EEPROM through IIC, but the download failed. The EEPROM is 24LC1025-I/SN. The ... Show More
haines
USB superspeed peripherals
Dear ifx teams: 1、usb的并口控制信号,就是USB_PHY_CTL【0-12】组内等长,误差±5mil;usb的并口数据,就是USB_PHY_DQ【0-31】组内等长,误差±5mil,这个等长合理吗? 2、USB_PHY_CLK和数据线等长还是和控制线等长? 3.并口的阻抗需要控... Show More
Stalker
USB superspeed peripherals
Hello, I am starting work with FX3 chipset, and follow appnote AP75705 example USB Bulk Loop Auto. I have compile the code; Program the board  via "Co... Show More
ly
USB superspeed peripherals
Hello, I am now using the USB mass storage device sample to check how cyusb3014 is enumerated as a device, when I do not insert any device in the Type... Show More
VediGovind
USB superspeed peripherals
Hi All, am working on ar1820 sensor  with CX3 controller .  here taking raw firmware in 10 bits of depth. it's working fine on some boards exactly out... Show More
fventuri
USB superspeed peripherals
I am working on a project where we would like to connect an ADC directly to the FX3 and send to the host only alternate samples (i.e. every other samp... Show More
zhangshun
USB superspeed peripherals
Hello, I have implement 2 virtual com port on the FX3 development board (CYUSB003-Kit), and they are running well. It would be nice if I can identify ... Show More
Translation_Bot
USB superspeed peripherals
The EEPROM of the CYUSB3014-BZXC cannot be burned into the firmware using IIC, every time the burn-in fails, the EEPROM used is 24LC1025-I/SN, and the... Show More
tetsu_8386
USB superspeed peripherals
Hi, @Ajeethkumar_P  I have encountered the same striping case discussed on this page, under the same MultiChannel DMA conditions.Since I am unable to ... Show More
jali
USB superspeed peripherals
Hello, I'm debuging the USB MSC on the CYUSB3014 board, I check the demo code(USBMassStorageDemo), it define the buffer on the ram, I want to write al... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.