Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Weiqi__Zhong
USB superspeed peripherals
CyU3PDmaChannelSetupSendBuffer这个函数在使用debug的时候出现了67的错误,请问这是什么原因导致的呢?并且,我想询问一下,在任何USB设备下,假如某一个端点设置成INT模式,主机是否会轮询这个端点,从而每当此端点有数据的时候,在主机的轮询下就会发送给主机??我需要完成... Show More
她说隔岸观火
USB superspeed peripherals

我想对CyBootprogrammer.img这个固件新加一条命令,所以我想知道这个固件的源码在哪里

TaKI_297676
USB superspeed peripherals
Dear Support Members   I defined mutichannel dma for stream as below (DMA Size is 16KB...as i think...) ====== #define STREAM_DMA_BUFFERS         6#de... Show More
Jakob
USB superspeed peripherals
Hello, I am searching for a solution, for my task. I want transfer a video signal from USB 3 to a 24 bit RGB-signal for a display. At first glance the... Show More
Osprey
USB superspeed peripherals
Unit has been in production for 6 years. Device will be listed in the Device Manager with Intel(R) 3.0 eXtensible Host controller. But has sporadic li... Show More
Translation_Bot
USB superspeed peripherals
Hi. I use the cyusb3014 in slavefifo mode to connect with the fpga chip, and after the power up , the system works well, but if i send vendor command ... Show More
zhouhuanan
USB superspeed peripherals
你好:我自己画了一块板子,我下载Cx3UvcOV5640.img程序到flash后,USB设备未能出现CX3-UVC的图标。这个IMG 我下载到开发板中是好使的。串口报错AppInit:MipicsiInit Err = 0x45。请问是什么原因?请问是否还要下载其它程序? 另外论坛里怎么不能搜索问... Show More
Translation_Bot
USB superspeed peripherals
linux driver
solved msg Solved
Hello, where can I find the linux driver framework for CYUSB 3014?smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%B6%85%E9%AB%98%E9%80%9FUSB%E5%A4%96%E... Show More
kanken6174
USB superspeed peripherals
After trying to debug some of the available C++ examples like BulkLpAutoCpp, i've found out that any C++ based project will not properly debug under o... Show More
Ankitvats
USB superspeed peripherals
Having the FPGA connected the FX3. And the data transaction happened between the FPGA and Host-app  using the bulk endpoints through Auto- DMA channel... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.