Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals

Recent discussions

Sort by:
Flute
USB superspeed peripherals
How CyAPI recovers data transmission after accidental USB reconnection 我们当前的解决方案是手动触发CYAPI通过Control End Point通道向CYUSB3014发送一条命令,CYUSB3014固件执行CyU3PDevi... Show More
rossihwang
USB superspeed peripherals
My hardware is a sensor connected to 3014 via DVP. The problem is the DVP signals are good(frame/line valid and the pixel clock).  And we can see the ... Show More
xwf72
USB superspeed peripherals
I designed a USB test module using CYUSB3014. This USB test module is used to test the USB HUB. The module runs the cyfxbulksrcsink example, and the c... Show More
jx
USB superspeed peripherals
CyU3PMemSet((uint8_t *)&dmaConfig,0,sizeof(CyU3PDmaChannelConfig_t));dmaConfig.size = CY_FX_UVC_STREAM_BUF_SIZE;dmaConfig.count = CY_FX_UVC_STREAM_BUF... Show More
Flute
USB superspeed peripherals
CYUSB3014 意外中断传输后不重启设备不刷新USB连接如何恢复传输? We have such a requirement: When CYUSB3014 is transmitting data in SuperSpeed mode, the USB is disconnected (for... Show More
mialc_1106291
USB superspeed peripherals
Hi, I've written a custom bootloader for the CYUSB3014-BZXC using the Cypress Boot API. We've been using this bootloader without issue for the past co... Show More
Rakesh
USB superspeed peripherals
Hi infineon team,  I port my source code ( build using 1.3.1) to 1.3.4 SDK. Upon compiling my code, I get an error message such as SYS_MEM overflowed ... Show More
Rakesh
USB superspeed peripherals
Hi infineon team, I am getting CyU3PDmaMultiChannelGetBuffer Failed with Timeout error code frequently when streaming 1080P resolution in YUV2 format.... Show More
Huton
USB superspeed peripherals
Hello. The driver resell work you worked on went well. Thank you. However, the upload to the Microsoft hardware dashboard failed after working with th... Show More
VastStar
USB superspeed peripherals
PMODE[2:0]选择的Z11,使用的EEPROM型号为24L1025I/SN(1024M/Microchip),使用elf2img.exe时加入了设置-i2cconf 0x1E,生成.img文件。再使用Control Centor将固件下载到EEPROM中,但失败了。 1.选择I2C EEPRO... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.
Top Solution Authors