Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

athreya
USB superspeed peripherals
Hi I am trying to grab frames from MIPI - USB3 using econ CX3 RDK attached with a custom sensor. The configuration is as below. Using a scope I can ve... Show More
KePa_4784036
USB superspeed peripherals
Hi community, I was just wondering if it is possible to access the build variables in the code I'm writing. I didn't find a way so far. At first, thos... Show More
aranin
USB superspeed peripherals
Our FX3-based device can be powered by battery, so USB is only needed to power it on until the switch over to battery as power source. An FPGA is conn... Show More
rossi
USB superspeed peripherals
Hello, I have developed firmware that operates as a USB 2.0 host on FX3.This firmware provides support for the HU205 UVC webcam as a device. Now, I ai... Show More
rossi
USB superspeed peripherals
Hello, I have two successfully running fx3 firmwares, one of which runs as a usb2.0 host(OTG) and the other as a device. For the new requirement, I ha... Show More
irki_4835741
USB superspeed peripherals
Hello,I am working with the CX3 Denebola Dev Kit. I implemented multiple framerate (30 and 60 fps) for VGA, following the discussion from this link =>... Show More
HaKe_1515226
USB superspeed peripherals
Our hardware product is built around the CYUSB3013 chip. To communicate with the device, the PC uses an isochronous endpoint. When we configure the de... Show More
ly
USB superspeed peripherals
Hi,Now that my USB enumeration is successful, I want to register a control transfer command to switch the usb connection speed freely between USB 2.0 ... Show More
DANSON
USB superspeed peripherals

What is the current consumption at each power pin of CYUSB3014-BZXI?

jack_Yang
USB superspeed peripherals
Dear technical support expert, I 'm study your KBA237926 article , it says the sensor AR1335 use on board oscillator as input clk. Can you kindly tell... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.