Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

Sort by:
chrec_4073846
USB superspeed peripherals
Hi All, I'm using cypress FX3 super speed USB device for my testing, I want to use it as a mutt device. Is it possible?Thanks,Chandralekha Show More
holec_1218441
USB superspeed peripherals
我想问一下,这个EZ USB Suite支持的Jlink GDB Server的版本有没有要求?我在segger官方找的jlink版本暂时只要V644a和V644b这个问题该如何解决? Show More
ethuc_3587321
USB superspeed peripherals
Hi,How can I make CyUSB3014 switch from a usb3.0 device to a usb2.0 device?Intel chipset if you connect a USB2.0 device and USB3.0 device will used di... Show More
siwrc_2591756
USB superspeed peripherals
HiI'm using the CyAPI API for performing asychronous bulk transfers between the host (running Windows 10) and a Cypress FX3.The FX3 is sending data to... Show More
gean_3054931
USB superspeed peripherals
Hello,we are using fx3 device(cyusb3035) with jtag segger.we are able to use jtag segger with fx3 but we need to program spi flash that is connected t... Show More
PoVe_3939176
USB superspeed peripherals
Im trying to connect customized USB 3.0 with PC but it is not recognizing  Kindly suggest to resolve the issue. Show More
majoc_2100616
USB superspeed peripherals
Making an open-source design for a hobby project I plan to sell . Making designs based on the wonderful design guidelines document, but I came across ... Show More
yogac_3765066
USB superspeed peripherals
Hello,I've Xilinx FPGA with fixed possibility to configure. So, I wanted to configure that FPGA via JTAG.Is it possible to use GPIO pins as JTAG pins,... Show More
AnWa_3863696
USB superspeed peripherals
Hi,I have followed the discussion FX3 UVC Extension Unit  and CX3 UVC extension unit ,only sample FX3 FW works well on UVC extension. For CX3 UVC exte... Show More
nich_4061921
USB superspeed peripherals
Hi guys! So, I finally got my fx3! Super excited  and I'm designing a super speed only device. I know that a possible release would have compliance is... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.