Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

Sort by:
Anonymous
USB superspeed peripherals
During development of a Chrome-application we have got problems, with our camera never seen in Apple OS or Windows.    The Linux V4L2 driver returns c... Show More
Sag
USB superspeed peripherals
Hey, What is the best way to update the FW on the CX3 while in SPI boot mode (USB on failure) after the 1st FW flash?When the SPI is empty, connecting... Show More
Rakesh
USB superspeed peripherals
Dear cypress team, i need to use GPIF II designer  with 24 bit data bus. but 24 bit option is not available in designer tool . can you explain why it ... Show More
Nzagone
USB superspeed peripherals
Hello, dear Infineon support community ! I am currently working on a custom UVC application based on AN75779 and CYUSB3KIT_003. To simulate data comin... Show More
KeWa_2323766
USB superspeed peripherals
We currently use FX3 for UVC application.  In road map,  SX3 is highlighted for UVC while FX3 is not. May I know the difference between FX3 and SX3?  ... Show More
mialc_1106291
USB superspeed peripherals
Hi, We have developed a custom PCB with the CYUSB3014-BZXC and we've noticed that sometimes when we connect the board to the PC using a USB 3 C to C o... Show More
VastStar
USB superspeed peripherals
对于slavefifoasync这个固件,想要在里面启用control endpoint,但是FPGA的信号线应该连接CYUSB3014的哪个引脚? 另外,请问在slavefifoasync这个固件中如何增加control endpoint的功能。   Show More
Yamuna
USB superspeed peripherals
Hi,  I'm using FX3S as a USB host controller. and I wanted to implement SDIO IO peripheral, I'm able to do SDIO initialization successfully. After tha... Show More
Magnus_P
USB superspeed peripherals
Hello!We are using the FX3 and the AN75779 in a customer camera project.For certain use cases we see the code executing gets stuck on the call to CyU3... Show More
Wellington
USB superspeed peripherals
Hi, We having trouble to receive frame when send two Frame Request two endpoint simultaneously. We are using window10 64x, CyAPI library. I am connect... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.