Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Translation_Bot
USB superspeed peripherals
I use VISUAL STUDIO to write programs and communicate with CYUSB3014. CYUSB3014 works in synchronous FIFO mode. Are there any detailed control procedu... Show More
azot_0
USB superspeed peripherals
Hi, Currently I use CyU3PI2cTransmitBytes/CyU3PI2cReceiveBytes. When I need to send only the preamble without data phase, i send one bye of 0x00 which... Show More
立月倪静
USB superspeed peripherals
CYUSB3065
solved msg Solved

求CYUSB3065芯片的原理图和PCB封装库文件

pbk
USB superspeed peripherals
Hello. When trying to create a new configuration project for the CX3 in the latest Eclipse EZ-USB suite 1.3.5 IDE, the tool reports the following erro... Show More
cx3develop
USB superspeed peripherals
I want to know the actual speed between the USB device and the host. It seems that the speed at which actual data can be fetched varies depending on ... Show More
tderensis
USB superspeed peripherals
Does the ThreadX implementation used in the EZ-USB FX3 SDK detect stack overflows? If so, what method does it use to recover? I would think it is one ... Show More
sasha
USB superspeed peripherals
Hi, I need to change the GPIF config during a runtime. I've read about sequence:1. GpifDisable()2. De initialize all the peripheral blocks.3. Reconfig... Show More
Translation_Bot
USB superspeed peripherals
CX3 wants to use the GPIO function at the same time as using the OV5640. No matter who defines these two functions first, the latter one will report a... Show More
Translation_Bot
USB superspeed peripherals
Why can't I download the schematic file?smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%B6%85%E9%AB%98%E9%80%9FUSB%E5%A4%96%E8%AE%BE/VD-USB-DENEBOLA-CA... Show More
Translation_Bot
USB superspeed peripherals
Using the CyfxDebugInit function alone status = cyu3puArtSetConfig (& uArtConfig, NULL); Cyu3pDebugPrint printing works well. Refer to apiretStatus = ... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.