Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

Sort by:
ankitvats846
USB superspeed peripherals
Hi,  I wanted to Flash the Fx3 Firmware First in RAM. And than write into the SPI Flash. Basically ,I wants when Firmware in SPI Flash is get corrupte... Show More
Nanda
USB superspeed peripherals
We are using CYUSB2304-68LTXI in our instrument. We have both USB Full speed and High Speed devices on the same hub.  On power up the USB Full speed d... Show More
rossi
USB superspeed peripherals
I'm writing USB 2.0 OTG UVC host firmware on FX3 and usb 2.0 web cam is used as device.  The traffics generated between PC and web cam were captured b... Show More
rossi
USB superspeed peripherals
Hello,  While receiving data from UVC camera in my USB 2.0 host firmware,  ocasionally 0x53(CY_U3P_ERROR_STALLED) errors were found after CyU3PUsbHost... Show More
subk1234
USB superspeed peripherals
Hi, I am using a CX3 Dev Kit to interface to an Omnivision OCSHA10 image sensor. I am debugging the quality of the image received from the sensor.  Wh... Show More
ZhBo_4667106
USB superspeed peripherals
Hello, I setup fx3 superspeed kit with FPGA board to test streamOUT example provided. Streamer and loopback functions well. I can transmit data and re... Show More
e_drouin
USB superspeed peripherals
Hi everyone! I have a product with an FPGA connected with a Cypress CYUSB3011 using a GPIF 16bits. The FPGA code is based on AN65974 and the firmware ... Show More
oguzandic
USB superspeed peripherals
Hello, I'm using CYUSB306X IC with deserializer (MAX9296) and serializer (MAX9295) structure. I can take stream without SerDes, with AS0149 MIPI board... Show More
qiwec_297866
USB superspeed peripherals
Hi    Now, i capture the total 65536 points of ad data in fpga fifo, and use a wire flag to indicate the fpga fifo is full(the flag state is 1, and th... Show More
Kevin_Lo
USB superspeed peripherals
Dear Sir/Madam, Our customer engineers is using USBBulkSourceSink Example to test and get the UART debug log to acquire the error code to analyzer iss... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.