Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Sort by:
tderensis
USB superspeed peripherals
We are attempting to adapt the example for the OV5640 to a different sensor which only as a RAW 10-bit bayer output.  Would it be possible to convert ... Show More
jali
USB superspeed peripherals
I used the demo code cyfxuvc_an75779,  hardware CYUSB3KIT-003  and ov7725, just change the resolution to 640*480, and GUID RGB565,  RUN this code, get... Show More
vhall2
USB superspeed peripherals
I am working with a GPIF to USB example that uses a "MANY TO ONE AUTO" DMA. This is similar to the UVC example but the ADC is a simple 16bit parallel ... Show More
Abhijeet
USB superspeed peripherals
I have created fx3 UVC application in EZ usb suite with sending video feed by DMA. now I want to add one usb interrupt for receiving string by android... Show More
Dineshkumar
USB superspeed peripherals
Hello, We are using CX3 - CYUSB3065-BZXI chip in our products and we are using some other chipsets in our design. Due to some design constraints, we h... Show More
HarryXia
USB superspeed peripherals
I am investigating if I can use EZ-USB FX3 chip to send voice data (80MBytes/second) from a acoustic array(FPGA) to Nvidia Jetson Xavier NX ( ARM64, L... Show More
NickNick
USB superspeed peripherals
Hi. If you build an example project in EZ USB Suite (attached), then everything works. But if I open the configurator and (without changing anything) ... Show More
UM
USB superspeed peripherals
I want to change the bus width to 32-bits in the AN75779 code example. When this is done how is the YUV2 format presented to the chip? In the 8Bit cas... Show More
Patrick0x400
USB superspeed peripherals
I'm using CYUSB3014 and xilinx zynq 7010 for my program. Is that any low-power function when there has not usb transfer events? I already try to add t... Show More
UM
USB superspeed peripherals
I want to use the Code found with the AN75779 to operate a non-Aptina sensor to produce an image. I do not want to use the I2C bus to communicate with... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.